The Right Fit

Complete water cooling systems (for example: Exos-2.5, PC5-1336, etc.)...
Rotbone
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Tue Sep 06, 2011 5:55 pm

The Right Fit

Postby Rotbone » Tue Sep 06, 2011 5:59 pm

Hello, I recently purchased a PC for my son from CyberPower. Long story short, I am not sending it back a second time. They are the worst I have every dealt with.

What I need to do is replace the bad water pump they installed. It stopped working once, sent back. Stopped working again. I want to make sure I am buying the right fit for this system. I want to make sure the pump I buy will handle 1 CPU block and 2 GPU blocks. I am an experienced computer tech, but I have been out of the loop for about 5 years now so I don't know much about the water cooling systems. I have drained the system and I am now ready to replace the junk. Please look at the PC specs and give me your input as to what size pump I need as to the flow rate, head pressure etc. etc.

Thank you

CPU: Intel(R) Core™ i7-990X Extreme Edition 3.46 GHz 12M Intel Smart Cache
LGA1366
CS_FAN: Maximum Enermax 120MM Case Cooling Fans for selected case (Maximum
Silent Operation) [+29] (1,000 RPM Black Color with No LED Enlobal Magnetic
Barometric Bearing 17 dBA)
HDD: 64 GB ADATA S501 V2 SATA III 6.0G/s Gaming MLC Solid State Disk (64GB x 2
(128GB Capacity) Raid 0 Extreme Performance)
HDD2: 2TB (2TBx1) SATA-III 6.0Gb/s 64MB Cache 7200RPM HDD (Single Hard Drive)
MEMORY: 12GB (2GBx6) DDR3/1600MHz Triple Channel Memory
MOTHERBOARD: (3-Way SLI Support) GigaByte G1.Guerrilla Intel X58 Chipset
SLI/CrossFireX Triple-Channel DDR3 E-ATX w/ 7.1 Creative X-Fi Xtreme Fidelity
Audio, Bigfoot Killer E2100 GbLAN, eSATA, USB3, 2x SATA3 RAID, 3 Gen2 PCIe, 2
OVERCLOCK: Ultimate OC (Ultimate Overclock 30% or more)
POWERSUPPLY: * 1,200 Watts - CoolerMaster Silent Pro 80 Plus Gold Power Supply
USB: Built-in USB 2.0 Ports
VIDEO: EVGA Liquid Cooling NVIDIA GTX Series PCIe Video (Liquid Cooling NVIDIA
GTX 590 Classified Hydro Copper 3GB 16X GDDR5 VRAM)
VIDEO2: EVGA Liquid Cooling NVIDIA GTX Series PCIe Video (Liquid Cooling NVIDIA
GTX 590 Classified Hydro Copper 3GB 16X GDDR5 VRAM)

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: The Right Fit

Postby Izerous » Wed Sep 07, 2011 10:50 am

A dual pmp-400 or pmp-450 unit would be best of course as overkill on cooling is always beneficial if you can afford it. However even a single PMP-400 or PMP-450 should be able to handle what you have listed just cooling the CPU and 2GPUs.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

Tuthsok
Water Pistol Grunt
Water Pistol Grunt
Posts: 21
Joined: Fri Jun 24, 2011 3:32 pm
Location: Victoria BC Canada

Re: The Right Fit

Postby Tuthsok » Wed Sep 07, 2011 2:06 pm

I have 2 PMP-400 pumps in series in a Koolance RP-401X2. At first I ran just a CPU block (Koolance 370) and could get 1gpm flow rate when running the pumps at 8v.

I then added a single EVGA 590 Hydro Copper and now have to run the pumps at max (12.7v via Koolance TMS-200) to get 1gpm.

I find the hydro copper blocks cool well but are very restrictive. I do not know what the effects of two of them would be on the flow rate of my loop.

As it stands things still stay nice and cool when I run the pumps lower at 9v, I am going more for a quiet system than being able to max my overclocks with water cooling.

Given the opportunity I may have gone with a pair of PMP-450s and the RP-452X2 reservoir if I knew those cards would affect flow rates this way.


Return to “Water Cooling Systems & Kits”

Who is online

Users browsing this forum: No registered users and 2 guests