About changing Exos 2.5 Fans

Complete water cooling systems (for example: Exos-2.5, PC5-1336, etc.)...
Igb
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Mon May 02, 2011 8:57 am

About changing Exos 2.5 Fans

Postby Igb » Tue Oct 04, 2011 10:52 am

Hi, im willing to do a very simple mod to my EXOS 2.5, essentially to reduce the loudness a bit, specially under heavy load.

My problem is that i haven't found detailed specifications of the control board, if there are strict current limits on the fan connectors, or any other information i should be aware of. I expect it to be starndard 3-pin voltage regulated fan connections, but i want to be sure, since most mods rewire the system completely

I assume the auto setting should work exactly as it was with this simple change. This is the board I'm finding if I'm right: http://www.koolance.com/water-cooling/p ... ct_id=1084

Many thanks in advance.

[Koolance] James
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 53
Joined: Mon Oct 24, 2011 2:26 pm

Re: About changing Exos 2.5 Fans

Postby [Koolance] James » Wed Oct 26, 2011 8:35 am

Hello Igb,

You found the correct control board. The total fan current limit on the PCB-EX004P is 3A. But each header is limited to 2A. Keep in mind that this board has only been tested with Koolance fans (which are PWM).

James


Return to “Water Cooling Systems & Kits”

Who is online

Users browsing this forum: No registered users and 1 guest