EX2-1055 Temperature Channels Switched?

Complete water cooling systems (for example: Exos-2.5, PC5-1336, etc.)...
jasonvp
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Thu Feb 13, 2014 8:28 am

EX2-1055 Temperature Channels Switched?

Postby jasonvp » Thu Feb 13, 2014 8:56 am

Hey folks -

I just installed my new EX2-1055, and found an interesting problem. It seems like the temperature sensor channels 1 and 3 are reversed, for some reason. If I connect a sensor to channel 1 on the slot adapter, the main unit sees it on channel 3. Likewise, if I connect that same sensor to channel 3 on the slot adapter, the unit sees it on channel 1. Channel 2 is seen as channel 2.

Has anyone seen that before? I assume that as long as I keep a sensor connected to channel 3 on the slot adapter, that the entire system will run fine. The unit thinks it's actually channel 1, and it appears to make the appropriate adjustments to the fan speeds as the temps rise.

Any ideas or thoughts?

Thanks!

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio

Re: EX2-1055 Temperature Channels Switched?

Postby Ace0751 » Mon Feb 17, 2014 7:35 pm

The circuits on the board could be reversed, things like that happen during production. As long as it's not causing any other issues I wouldn't worry about it that much.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case


Return to “Water Cooling Systems & Kits”

Who is online

Users browsing this forum: No registered users and 1 guest