Customer Case Gallery

Complete water cooling systems (for example: Exos-2.5, PC5-1336, etc.)...
Knuckles6
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 58
Joined: Tue Sep 30, 2008 7:00 am

Re: CASE GALLERY

Postby Knuckles6 » Wed Sep 16, 2009 3:03 pm

You really need to do something with the photos, scale them down or post thumbnails. You can only see a small part of the system. Nothing of the insides.

User avatar
omegastitch
Garden Hose Sharpshooter
Garden Hose Sharpshooter
Posts: 173
Joined: Sat Sep 12, 2009 11:08 am
Location: Tooele, UT
Contact:

Re: CASE GALLERY

Postby omegastitch » Wed Sep 16, 2009 3:22 pm

I have a stray question. how do you insert the images into the forum posts?
Last edited by omegastitch on Wed Nov 04, 2009 9:55 am, edited 1 time in total.
omegastitch

If ignorance is bliss, please let me die unhappy.

Dayeo78
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 37
Joined: Wed Apr 29, 2009 9:37 am

Re: CASE GALLERY

Postby Dayeo78 » Wed Sep 16, 2009 7:34 pm

Bambihunter,
Thanks for the CF2 pic's. Now I'm seeing a problem on the placement of the NB/SB blocks with my dual board 295's. Refresh my memory is the NB the plate just below the CPU or the one in between the three PCI-E slots?

Dayeo78
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 37
Joined: Wed Apr 29, 2009 9:37 am

Re: CASE GALLERY

Postby Dayeo78 » Wed Sep 16, 2009 7:44 pm

Sorry for the double post. Bambihunter are you using a pair of 125's for both the NB and the SB? If so that explains where my problem would be if what I saw was your bridge plates...

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: CASE GALLERY

Postby bambihunter » Thu Sep 17, 2009 9:41 am

Knuckles6 wrote:You really need to do something with the photos, scale them down or post thumbnails. You can only see a small part of the system. Nothing of the insides.


bambihunter wrote:****edit - good lord, sorry for the size of the pics :o . I will edit those in the next day or so and replace the pics****



Yep, I knew that right after I posted that (thus my edit at the top of the original post). My pictures usually scale most other places I go, I don't know why they don't here on the Koolance forums. I see they also still haven't fixed the long post bouncing while typing issue either.


Dayeo78, I added another close-up of the northbridge area. I was using the CHC-125's but one of them started to leak internally so I swapped them out for CHC-122's I think.
On the CHII, the NB chipset is between the first PCI-E x16 slot and the CPU. The SB chipset is the one that is right in the way if you want to use the middle PCI-E x16 slot. If a person wanted to do tri-sli with this setup, I would recommend finding a passive NB cooler of an older Nvidia board and using it for the SB. If I remember right, the SB on this series puts out at a max of 12watts of heat. Instead of doing that though, the best thing would be just use a pair of GTX295's for quad-SLI (like it sounds like you are using).
If I didn't have to go out the back of the PC for the power supply tubing I think I would remove the waterblock now because I really would like to add another video card for more folding power. This rig right now is making above 9k ppd for each GTX280 and between 4k and 5k ppd depending on the WU.
When the GTX300 series comes out I might move these two GTX280's to my PC3-720 and get a pair of the new ones if they are as good as everyone claims.
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

Dayeo78
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 37
Joined: Wed Apr 29, 2009 9:37 am

Re: CASE GALLERY

Postby Dayeo78 » Thu Sep 17, 2009 3:55 pm

Thanks again bambihunter, going to try the CHC-120-V06 for the SB and hopefully that clear the primary GPU. If everything goes to plan I'll have my pictures here next month to join the ranks.

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: CASE GALLERY

Postby bambihunter » Fri Sep 25, 2009 7:31 am

Dayeo78 wrote:Thanks again bambihunter, going to try the CHC-120-V06 for the SB and hopefully that clear the primary GPU. If everything goes to plan I'll have my pictures here next month to join the ranks.


Your primary GPU is not the problem, neither is GPU2 (which is the 3rd physical slot). The problem is the middle PCI-e x16 slot (which is the one you would use for your 3rd GPU - I know, they should be in order but they are not).
So to clarify, if you are running two or fewer PCI-e x16 video cards you will be fine with any southbridge chipset block. The problem only arises when you want to put in the 3rd card. If I were to build my system right now, I would put in a pair of GTX295's (for quad-sli using only 2 slots).
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

Dayeo78
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 37
Joined: Wed Apr 29, 2009 9:37 am

Re: CASE GALLERY

Postby Dayeo78 » Fri Sep 25, 2009 9:10 pm

Thanks again Bambihunter.

Mikesnow
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 76
Joined: Sun Jul 19, 2009 11:39 pm

Re: Customer Case Gallery

Postby Mikesnow » Sat Oct 17, 2009 9:45 am

So heres my new PC video.

Koolance parts used are:
1 x INS-FM17 INS-FM17 Coolant Flow Meter & Adapter Board
3 x VID-428 VID-428 (GeForce GTX 280/260)
1 x CPU-345AC CPU-345AC (CPU), Acrylic
13 x NZL-V13KG Nozzle Pair, G 1/4" Compression [For ID: 13mm (1/2")]
5 x NZL-L13P Nozzle Pair, G 1/4" Swivel Angled [For ID: 13mm (1/2")]
1 x RP-1000BK Reservoir and Pump, Black
1 x SEN-AP005PB Coolant Temperature Sensor
1 x VLV-13TSPL Drain Valve [ID: 13mm (1/2")]
1 x MB-EVX58CF MB-EVX58CF (EVGA X58 Classified)
1 x BKT-CP345 Fixed Post Bracket for CPU-345
3 x BKT-VD001P Single Slot GeForce Bracket
1 x MVR-PLTEV104 MVR Heat Transfer Plate, Stepped 104mm
1 x MVR-100 MVR-100 (MB VReg)
1 x CNT-VDA2 Dual VID Connector, Adjustable 1 Slot Spacing
1 x CNT-VDA34 Dual VID Connector, Adjustable 3-4 Slot Spacing
1 x COM-M38 Cold Cathode, 12" UV Dual
1 x HX-1020 Radiator, 3x120mm, Aluminum Vert.
1 x HX-422 Radiator, 1x120mm, Aluminum Vert.
4 x FAN-12025HBK Fan, 120x25mm (FAN-12025HBK)
1 x TMS-200 TMS-200 Software Thermal Interface Controller
8 x HOS-13CL Tubing, Clear PVC, 1ft/30.5cm [ID: 13mm (1/2"); OD: 16mm (5/8")]
6 x SPR-13RD Tubing Spring Wrap, Red [For OD: 16mm (5/8")]

Unfortunately, my tms-200 was messin up so have to RMA it, but once I get it back and working again I intend on getting the expanssion board for it and splitting the loop into 2 loops.
Asus Rampage IV Extreme
Intel Core I7-3930K w/CPU-360
32GB Patriot Viper3 Series 2133MHz Ram
2x Corsair Performance Pro CSSD-P256GBP-BK (Raid0)
2x Western Digital - 1TB HDD (Raid1)
EVGA GTX 680 w/VID-NX680
Silverstone ST1500 PSU
Corsair Obsidian 800D

User avatar
HELLFIRETOYZ
Tactical Bucket Splasher
Tactical Bucket Splasher
Posts: 301
Joined: Sat Nov 01, 2008 8:56 pm
Location: Peoria, AZ
Contact:

Re: Customer Case Gallery

Postby HELLFIRETOYZ » Wed Nov 04, 2009 3:50 pm

Thought I'd join in and show off some of my rig. This is build was my first build ever and over the years it has been remodeled I don't know how many times.

Image

Image

Image

Image

Image

Image

Image

I have plans over the weekend to install an INS-FM17 and Thermal Control Board. I recently added some new parts and redesigned my loop hoping for better temps and a stronger flow rate. I'll post my stats on that project sometime next week.
Hellfire - multi-mission, and multi-target precision-strike capability weapon system, "fire-and-forget!"

BFG GTX285 OC'd 3-Way Blocked
Asus P6T7 SuperComputer Blocked
i7 920 @ 4.21Ghz Blocked
Corsair DDR3 1600 - 6Gb
OCZ Vortex SSD 120


Return to “Water Cooling Systems & Kits”

Who is online

Users browsing this forum: No registered users and 1 guest