Diference between two QD3 quick disconnect!!

Fittings, nozzles, quick-disconnects, speed controllers, power supplies, & everything else...
Koolobus
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Sat Oct 05, 2013 4:10 am

Diference between two QD3 quick disconnect!!

Postby Koolobus » Sat Oct 05, 2013 4:25 am

Hello,

I've googled this but no answer founded, so I'm here if anyone can help me :)

I would like to know what s the diference between the QD3-MFG4-P-BK and the QD3-MG4-BK ?


Image Image

I see that they have different G1/4", if there is no difference which one is beter fot the cpu block (I have the EKWB spremacy waterblock nikel/acetal)?

thanks for your help

Undesirable
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Thu May 08, 2014 6:42 pm

Re: Diference between two QD3 quick disconnect!!

Postby Undesirable » Thu May 08, 2014 6:58 pm

The QDC with the larger diameter thread (QD3-MFG4-P-BK) is a female G1/4 (other fittings screw into it, such as compression fittings), also that large metal hexagonal screw ring around the thread can be manipulated independently and allows it to be mounted on bulkheads, such as holes in a PC case, for connecting external radiators, although you don't have to use it in this fashion. The actual quick disconnect end, however, is male.

The QDC with the smaller diameter thread (QD3-MG4-BK) is a male G1/4 fitting and screws directly into female G1/4 ported radiators, reservoirs etc. The quick disconnect end on this part is also male.


Return to “Fittings, Nozzles, Quick-Disconnects, Misc.”

Who is online

Users browsing this forum: No registered users and 2 guests