How to calibrate INS-FM17 with Aquaero

Fittings, nozzles, quick-disconnects, speed controllers, power supplies, & everything else...
Santiago
Water Pistol Grunt
Water Pistol Grunt
Posts: 24
Joined: Fri Jan 16, 2009 9:58 pm

Re: How to calibrate INS-FM17 with Aquaero

Postby Santiago » Mon Apr 13, 2009 9:45 am

Why is it so hard to get a straight answer :)

He needs to know pulses per minute. I see a math head post and lots of references to "the manual" which does not list pulses per minute. How about someone make that translation? I'm sure it would be helpful for others as well.

Thanks :D

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: How to calibrate INS-FM17 with Aquaero

Postby [Koolance] Tim » Wed Jun 03, 2009 4:01 pm

I'm not particularly sure what information is missing. If you bypass the INS-FM17 multiplier board and read the flow meter directly, this is the pulse frequency chart (in the user manual/website):

Image

As Izerous mentioned, it would be pulse x 3.285 for 10-13mm ID, or 3.627 for 6mm ID.

However, if you are connecting to the included multiplier board, the pulses/liter should be (x10) 32.85 for 10-13mm ID, and (x9) 32.64 for 6mm ID.

Please post back if this works.

brunediddy
Water Pistol Grunt
Water Pistol Grunt
Posts: 13
Joined: Sun May 24, 2009 1:59 am

Re: How to calibrate INS-FM17 with Aquaero

Postby brunediddy » Tue Jun 09, 2009 11:53 pm

Out of curiosity,

hows is it that 3/8 and 1/2 ID flowrates are equal? Is it because the sensor itself has smaller ID then the 1/2 therefore the flow makes no difference?

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: How to calibrate INS-FM17 with Aquaero

Postby [Koolance] Tim » Wed Jun 10, 2009 5:05 pm

Yes, our G 1/4" threaded sockets have an internal diameter of 3/8". With a short, low-restriction component like the flow meter, the impeller rotation should not change much if the in/out tubes are 1/2" or 3/8" ID.

Top Nurse
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Aug 04, 2009 3:30 am

Re: How to calibrate INS-FM17 with Aquaero

Postby Top Nurse » Fri Sep 11, 2009 1:28 am

The correct pulses per minute out of the flow meter (without the multiplier board) is 197 for the Aquaero. You hook up one wire to the ground and the other wire to the RPM pin on the Aquaero. More information can be found here.

astrodanco
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 59
Joined: Wed Jul 01, 2009 7:10 pm
Location: San Diego, CA

Re: How to calibrate INS-FM17 with Aquaero

Postby astrodanco » Fri Sep 11, 2009 7:07 pm

As has clearly been stated above, for 10mm ID or larger, LPM = 0.3044 * HZ.

LPM = Liters per minute.
HZ = Pulses per second aka PPS.

To solve for HZ, substitute 1 for LPM and divide both sides by 0.3044.

HZ = 1 / 0.3044.

Then to turn HZ (PPS) into the number of pulses per minute (PPM), multiply by 60.

PPM = HZ * 60

197 = (1 / 0.3044) * 60

That gives 197.1... (and so on, we really only have four significant digits to work with).

197 is likely close enough.
Core i7 920 (D0) @ 4.0Ghz, P6T Deluxe V2 (1003), 12GB CM3X2G1600C7 @ 1600 7.7.7.20 2T, ATCS 840, Antec TPQ 850, Radeon 4850, TMS-200+EB200+FM17, EK Supreme HF, EK-D5 dual top, 2X MCP-655-B, MCR-320, 6X Skythe D1225C12B5AP-15, Durelene tubing, BP fittings.

lexus3x
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sat Oct 31, 2009 9:35 am

Re: How to calibrate INS-FM17 with Aquaero

Postby lexus3x » Sat Oct 31, 2009 9:51 am

my loop
i use 1/2" (13mm) ID, 3/4" (19mm) OD tubing
t3
1. subloop
T3LO
D-Tek FuZion v2 + Koolance QDC(VL3N-F13-19S + VL3N-F13-19S)
QDC(http://www.aquatuning.de/product_info.php/info/p2722_Schnellverschluss-CPC-12-7mm-Kupplung.html + http://www.aquatuning.de/product_info.php/info/p2724_Schnellverschluss-CPC-12-7mm-Stecker-mit-Schottverschraubung.html)
MORA 2 radiator
QDC(http://www.aquatuning.de/product_info.php/info/p2722_Schnellverschluss-CPC-12-7mm-Kupplung.html + http://www.aquatuning.de/product_info.php/info/p2724_Schnellverschluss-CPC-12-7mm-Stecker-mit-Schottverschraubung.html)
Koolance INS-FM17 Coolant Flow Meter & Adapter Board
T3LI
2. subloop
T3HO
parallel 3* EK-FC285 GTX PCB Rev.2 SLI - Nickel/Acetal + Koolance QDC(VL3N-F13-19S + VL3N-F13-19S)
Swiftech MCW-NBMAX + Koolance QDC(VL3N-F13-19S + VL3N-F13-19S)
T3HI
Image

I take readings this device

Image
http://www.koolance.com/water-cooling/product_info.php?product_id=740
And I have such result
D5 1st speed 1320 RPM
D5 2st speed 1811 RPM
D5 3st speed 2395 RPM
D5 4st speed 3078 RPM
D5 5st speed 3860 RPM

what my flow rate in litres per hour?

lexus3x
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sat Oct 31, 2009 9:35 am

Re: How to calibrate INS-FM17 with Aquaero

Postby lexus3x » Sat Oct 31, 2009 10:04 am

ore litres per minute?

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: How to calibrate INS-FM17 with Aquaero

Postby [Koolance] Tim » Fri Nov 06, 2009 12:12 pm

Are you using an Aquaero? This thread is for customers connecting the INS-FM17 to the Aquaero.

If you're connecting the INS-FM17 to the motherboard or a regular fan controller, the RPM's represent mL/min. This is described on the product's web page and in the user manual.


Return to “Fittings, Nozzles, Quick-Disconnects, Misc.”

Who is online

Users browsing this forum: No registered users and 2 guests