RAM-33 Pressure Drop

Hard Drive & RAM water cooling blocks...
Sleepdep247
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Wed Oct 07, 2009 8:53 pm

RAM-33 Pressure Drop

Postby Sleepdep247 » Wed Oct 07, 2009 9:03 pm

I'm looking for the PSI impact these blocks will have on a loop in this configuration:
Image

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: RAM-33 Pressure Drop

Postby [Koolance] Tim » Fri Oct 16, 2009 3:06 pm

While we have not posted the flow curves for RAM-33 yet, they are roughly similar to a chipset cooler with 6mm nozzles. It is a limitation of the width provided between DIMM slots on most motherboards. However, the RAM-33 is a bit less restrictive than the RAM-35.

For a 10-13mm ID system with moderate flow (4L/min+), we would recommend splitting RAM-33 into parallel (smaller ID) paths when there is more than 2 in the loop.

HOSH
Water Pistol Grunt
Water Pistol Grunt
Posts: 18
Joined: Thu Aug 12, 2010 5:19 am

Re: RAM-33 Pressure Drop

Postby HOSH » Tue Jan 25, 2011 7:15 pm

Thanks for the info, can this be added to the RAM-33 page? Also by the way, I still do not see the flow rates for the RAM-33 yet.

But running the PMP-450 @ 24V we can push 18.9L/min at max and 13mm ID tubing, so what would that translate to a 4, 6, 8, and 12 configuration/limitations be?

So should we push the 13mm into two or three 6mm ID paths? With the ideal of making the 6mm paths nearly the same length to keep the flow the same through them?

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: RAM-33 Pressure Drop

Postby Izerous » Wed Jan 26, 2011 9:04 am

There will be posts about this elsewhere but 3x6mm hosing is ~= to 1x10mm hosing for throughput. So in theory a 13mm hose could split to 4x6mm hoses but clearances would start being an issue unless you used regular barbs instead the of the superior compression barbs. The more you optimize for flow in this situation the more hoses and crowed it is going to get.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram


Return to “Water Blocks - Hard Drive & Memory”

Who is online

Users browsing this forum: No registered users and 1 guest