I am using corsair dominator, and was wondering if anyone had any experience about the ease with which the heat spreaders can be removed? The fins on top are secured by three screws going down into the top of the heat spreader. After the fins are removed, will the spreaders come away easy or are that attached in a way that makes it impossible to remove without damaging the modules themselves?
I am happy enough to take my time and do it slowly if it is possible, if it isn't possible, would prefer not to try, and wait to add the RAM cooling until I upgrade the RAM and can then get something with removable spreaders.
Advice about Corsair Dominator
-
- Water Pistol Grunt
- Posts: 3
- Joined: Sat Nov 29, 2008 6:01 am
-
- Water Balloon Grenadier
- Posts: 59
- Joined: Thu Apr 09, 2009 5:17 am
Re: Advice about Corsair Dominator
do not do it, they are chemically bonded on and can (and have done lots of times) pull the ram chips off the board.
-
- Water Pistol Grunt
- Posts: 3
- Joined: Sat Nov 29, 2008 6:01 am
Re: Advice about Corsair Dominator
Ok, thanks, I'll leave them for now. When I upgrade the RAM, I'll hunt around for something that has easily removable heat spreaders.
- HELLFIRETOYZ
- Tactical Bucket Splasher
- Posts: 301
- Joined: Sat Nov 01, 2008 8:56 pm
- Location: Peoria, AZ
- Contact:
Re: Advice about Corsair Dominator
I've found the best way to pull the heatsinks off the Dominator and similar modules is to use 90%+ isopropyl alcohol. Letting them soak in an alcohol bath for several hours will dissolve the bonding agents. With this method I have never had any chips pulled off the modules.
Hellfire - multi-mission, and multi-target precision-strike capability weapon system, "fire-and-forget!"
BFG GTX285 OC'd 3-Way Blocked
Asus P6T7 SuperComputer Blocked
i7 920 @ 4.21Ghz Blocked
Corsair DDR3 1600 - 6Gb
OCZ Vortex SSD 120
BFG GTX285 OC'd 3-Way Blocked
Asus P6T7 SuperComputer Blocked
i7 920 @ 4.21Ghz Blocked
Corsair DDR3 1600 - 6Gb
OCZ Vortex SSD 120
-
- Fire Hydrant Gunner
- Posts: 375
- Joined: Tue Sep 16, 2008 2:05 am
- Location: Manila, Philippines
Re: Advice about Corsair Dominator
If you want to use the Corsair H30 block you can simply remove the fins from the top of the modules and sit the block on top. It's not as elegant as the Koolance system in terms of direct cooling but I've used it for months with no problems.If you want to use the Koolance RAM blocks you could check out OCZ memory as they tend to come apart without drama.
-
- Water Balloon Grenadier
- Posts: 59
- Joined: Thu Apr 09, 2009 5:17 am
Re: Advice about Corsair Dominator
with it being memory the block ontop method would work very well for cooling the modules rather then voiding the lifetime warranty you get with corsair, my cooling fan kicks in at 50 degrees at 50% and cools them back to 30 in under a minute so it does not take much to keep them cool.
Return to “Water Blocks - Hard Drive & Memory”
Who is online
Users browsing this forum: No registered users and 1 guest