VelociRaptor Watercooling?

Hard Drive & RAM water cooling blocks...
tbully
Water Pistol Grunt
Water Pistol Grunt
Posts: 11
Joined: Tue Dec 16, 2008 2:01 pm
Contact:

VelociRaptor Watercooling?

Postby tbully » Tue Dec 16, 2008 2:05 pm

Has anyone had any luck using watercooling with these?

http://www.newegg.com/Product/Product.a ... 6822136260

I plan to put 4 in my PC4-1036BK and want to cool as much of my gear with water as possible.

Thanks.

weirdguyxp
Water Pistol Grunt
Water Pistol Grunt
Posts: 5
Joined: Mon Dec 08, 2008 2:07 pm
Location: USA
Contact:

Re: VelociRaptor Watercooling?

Postby weirdguyxp » Thu Dec 18, 2008 11:22 am

Yes, I have had luck water cooling these. I have 4 300g Raptors in RAID5. I use HD-57s, one Raptor on each side of the HD57. It works perfectly no problems having the HDs fit. I use the right angle 10mm fittings and have no clearance issues. Hope this helped.
My System:
Case - PC1336BK
MB - ASUS Rampage II Extreme - CHC-122 on NB
CPU - CORE i7 965 EXTREME - CPU-350
VIDEO - 3x EVGA GTX 280 SSC - 3x VID-428
RAM - 12GB 6x2GB OCZ DDR3-1600 - 6x RAM35
HD - 4x WD Raptor 300g 10k RPM - 2x HD-57
PSU - Tagan BZ 1300W

tbully
Water Pistol Grunt
Water Pistol Grunt
Posts: 11
Joined: Tue Dec 16, 2008 2:01 pm
Contact:

Re: VelociRaptor Watercooling?

Postby tbully » Thu Dec 18, 2008 11:24 am

weirdguyxp wrote:Yes, I have had luck water cooling these. I have 4 300g Raptors in RAID5. I use HD-57s, one Raptor on each side of the HD57. It works perfectly no problems having the HDs fit. I use the right angle 10mm fittings and have no clearance issues. Hope this helped.



This helped, indeed! Thank you!

A few experts at Koolance mentioned that it wasn't possible or difficult at best.

Thanks again.

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA
Contact:

Re: VelociRaptor Watercooling?

Postby [Koolance] Tim » Tue Dec 23, 2008 12:58 pm

Cooling the entire product (lower than air) through its stock heat sink using an HD-57 or HD-60 might be doable since it uses the 3.5" format. But I would wonder about the overall efficiency of this caused by a series of heat transfer points, and the distance between the heat sources and actual liquid.

If you got a negative reply from Koolance, I think we probably assumed you would disassemble the 2.5" drive from the 3.5" stock heat sink and attempt to attach that to a water block. Our current HD products do not have ready mounting positions for 2.5" drives. You would need to find some way to keep the drive abutting the cooler.

tbully
Water Pistol Grunt
Water Pistol Grunt
Posts: 11
Joined: Tue Dec 16, 2008 2:01 pm
Contact:

Re: VelociRaptor Watercooling?

Postby tbully » Tue Dec 23, 2008 1:11 pm

Tim -

This makes sense. The response wasn't negative, really. It was more of a "hmmm, we don't think / know if this is possible".

Your comment on efficiency also is interesting. You're right, the source of the heat is not near the actual heatsink.

User avatar
KingPenguin
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 49
Joined: Mon Sep 29, 2008 9:50 pm
Location: Indianapolis, IN
Contact:

Re: VelociRaptor Watercooling?

Postby KingPenguin » Tue Dec 23, 2008 1:38 pm

I wonder if any of the liquid cooling companies are going to start offereing a solution for the 2.5" format VelociRaptors. They run very cool anyway but it is always nice to have options.
Case: PC2-601BLW
CPU Block: CPU-200G
NB Block: CHC-A03
GPU Block: GPU-180-H06
PSU: ULT-XF600
GPU: BFG: AGP: 7800 GS OC
CPU: Northwood: P4Ht 3.0GHz
DDR RAM: Kingston(1GB): PC3200(x4)
MoBo: Asus P4C800E Deluxe
HDs (RAID0): WD500(x2)(SATA1): WD320(x2)(EIDE)

User avatar
Malevolent
Water Pistol Grunt
Water Pistol Grunt
Posts: 14
Joined: Wed Sep 17, 2008 5:09 am
Location: Alaska
Contact:

Re: VelociRaptor Watercooling?

Postby Malevolent » Tue Jan 27, 2009 12:55 am

tbully wrote:Has anyone had any luck using watercooling with these?

http://www.newegg.com/Product/Product.a ... 6822136260

I plan to put 4 in my PC4-1036BK and want to cool as much of my gear with water as possible.

Thanks.


For those who are not familiar with the Western Digital VelociRaptor 300GB Hard Drive and plan to purchase them, take note that there is two different types. Model #: WD3000GLFS is the older style that has the connections in the center of the drive and is known to cause some grief on certain configurations such as water cooling blocks and external enclosures. The main complaint is not having the ability to use them as swappable drives due to the fact that the connections do not match traditional SATA 3.5 drives. Model #: WD3000HLFS is the updated version that has connections matching traditional SATA drives that should take care of the previous problems encountered with the GLFS model. I use the HLFS model with my Koolance HD-60 cooling block and 1/4" Swivel Angled without any issues.

*Note* I did remove the mounting frame that came with the drive and made my own aluminum 3.5" custom mounting frame to match my MOD Design and also create better heat transfer to the Koolance HD-60. Unless you have the ability to create a better 3.5" mounting frame for your 2.5" VelociRaptor drive, I recommend you keep the drive stock and not use water cooling as it stays pretty cool as it is.
Asus Rampage Extreme
Intel Core 2 Extreme QX9770 CPU-350
Corsair XMS3 DHX 8GB
Sapphire Radeon HD 4870 X2 (X2) VID-487X2
WD VelociRaptor 300GB (X4) HD-60
Water Cooled by Fluid XP+ EXT (Black)
PMP-450(COV-PMP450A), CTR-CD10BK, INS-FM17,
Koolance 1300/1700W

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma
Contact:

Re: VelociRaptor Watercooling?

Postby bambihunter » Tue Mar 31, 2009 5:19 pm

With SSD's just around the mainstream corner I would wonder if anyone will bother with watering them since they do indeed run cool. I have been toying with the idea of a SAS card & drives. They have became quite cheap and outperform the Velociraptors by a fairly large margin. I bounce back and forth though since the aforementioned SSD's are getting better and cheaper and have speeds that will blow away any conventional disks. If they can extend the write life the hard drives as we know them will be dead I think... :ugeek:
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

Izerous
Rain Maker
Rain Maker
Posts: 1183
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada
Contact:

Re: VelociRaptor Watercooling?

Postby Izerous » Wed Apr 01, 2009 7:26 am

I already ran into the issue with the 2 different formats. Ordered a new 1U server for the office and the company we ordered through had sent the wrong format for the drives. They sent the older ones. I ended up keeping them anyways and just ordering 2 of the newer ones for the server and tossed the older format into my case at home.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

bobmac606
Water Pistol Grunt
Water Pistol Grunt
Posts: 10
Joined: Mon Mar 30, 2009 8:19 pm
Contact:

Re: VelociRaptor Watercooling?

Postby bobmac606 » Thu Apr 02, 2009 9:41 am

FYI, SSD Drives, by the time you make or get an adapter for them, you have spent a bit of money, then water cool them. Mine has been running for about 3 months and with a case fan on it feels as cool as when I put it in. These things run cool from the start and man they are fast, just writing to them takes a shade longer than the read. This year OCZ is supposed to have a 1T out, that should lower the pricing for the rest. But, I remember a 30 MEG RLL encoded drive cost roughly the same as a 120 Gig now. :) BTW, the heat sink on my VelociRaptor and a case fan keeps it nice and cool.

Cooler Master Cosmos
RP-1000
VID-428 (x2)
CPU-340
HX-1020 Rad
EHX-1020
Intel 920 I7 OC'd to 4.2 GHZ
EVGA X58 Motherboard
1 OCZ 120 SSD, 1 WD VelociRaptor 300GB, 2 X WD 1TB 7200 RPM 32MB Cache, 1 WD 1TB (Green) External E-SATA Backup Drive
Vista Ultimate 64
12 GB CORSAIR XMS3 SDRAM DDR3 1600 (PC3 12800)
2 EVGA GTX260's
1 Loop: CPU, both GPU's, MB-EVX58, MVR-40 using 1/2 inch tubing


Return to “Water Blocks - Hard Drive & Memory”

Who is online

Users browsing this forum: No registered users and 1 guest