Anyone have any pics of multiple Koolance HD Blocks in pc?

Hard Drive & RAM water cooling blocks...
bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby bambihunter » Thu Jul 16, 2009 10:23 am

I am considering using multiple HD blocks in a PC5-1336 (LianLi V2100 series) case. I am thinking of using multiples of them to cool only a single drive because I don't like the looks of the drives flipped back and forth, plus it can't be easy to wire. Is the spacing between the drives enough to use one of those blocks under each drive?

Anyway, if you have ANY pics of a similar case with EITHER of Koolance's HD blocks please post them. I'd like to see how you did them.
Thanks.

P.S. With SSD's becoming more and more mainstream maybe this isn't a wise investment, but I think rotating drives will be with us for another decade. I just bought 4 2tb drives for my media center to put in RAID-0 so I guess I am in it for a while. ;)
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

H2O-Cooled
Water Pistol Grunt
Water Pistol Grunt
Posts: 4
Joined: Tue Jul 28, 2009 10:00 am

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby H2O-Cooled » Wed Jul 29, 2009 2:01 pm

/bump

I'm interested as well....




anyone??
eVGA 750i FTW
Q6600
4GB RAM
Asus GTX260
<budget system with a lil oomph>

JuanPabloCuervo
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 33
Joined: Sat Aug 01, 2009 8:42 am

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby JuanPabloCuervo » Thu Aug 13, 2009 9:30 am

i love koolance,
have a near 100% complete koolance system,.
but i think thermaltake aquabay m4 is much better sollution.
i have 4x aquabay m4.

MCP
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 46
Joined: Tue Oct 21, 2008 1:30 pm

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby MCP » Thu Aug 13, 2009 9:57 am

Be careful using koolance equipment with those thermaltake drive coolers.

If you're using a koolance aluminum rad, you're going to have corrosion problems since the thermaltake piping is copper.

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby [Koolance] Tim » Fri Sep 25, 2009 11:11 am

There are some installed pics (in Lian-Li Chassis) at http://www.koolance.com/product_wizard/ ... e_help.php

JuanPabloCuervo wrote:i think thermaltake aquabay m4 is much better sollution.


That product is not likely to cool better than ours. It's copper pipe attached to a solid plate, whereas we are using a single-piece cooler (Hydra-Pak for the HD-57, or stainless steel for the HD-60). Our water blocks only mount to the bottom portion of the hard drive, so they can easily be converted to 5.25" bays with a standard drive bay adapter like this one:

drive_adapter.jpg

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby bambihunter » Fri Sep 25, 2009 11:49 am

I saw those Tim. I was hoping someone would have some pics with them all in a row with one on each drive instead of flipping every-other-one upside down. I'd also like to see what they'd look like with the cables on them. It is hard to visualize it with the sata and power wires connected along with all the blocks and tubing.
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

cybertank
Water Pistol Grunt
Water Pistol Grunt
Posts: 4
Joined: Wed Apr 15, 2009 9:46 am
Location: Toronto
Contact:

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby cybertank » Wed Jan 27, 2010 8:18 am

Here are mine...

IceHappy
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 32
Joined: Fri Sep 25, 2009 9:37 am

Re: Anyone have any pics of multiple Koolance HD Blocks in pc?

Postby IceHappy » Wed Feb 17, 2010 2:41 pm

thank you to everyone who posted as I am trying to come to terms with what kind of Hdd waterkooler to use and it seems like the only compatible solution is the Koolance solution.

I only wished that Koolance made a 5.25 bay enclosed Hdd kooler that not only is a waterblock but also a hdd silencer!!!!

An example of what I mean is this AquaDrive Dual in which XtremeComputing has rated it excellent see below link!

http://www.xtremecomputing.co.uk/review.php?id=272&page=5

However both Bambihunter and Hellfiretoyz both told me that Aluminum won't play nicely with Koolance kit..... :shock:

I never took Chemistry in HS or college ergo metal ignorant but not ignorant enough not to ask before screwing my system :D


Return to “Water Blocks - Hard Drive & Memory”

Who is online

Users browsing this forum: No registered users and 2 guests