New DIY "Priceless"

Do-it-yourself and user modifications...
LarryLuke
Water Pistol Grunt
Water Pistol Grunt
Posts: 4
Joined: Fri May 08, 2009 1:42 pm

New DIY "Priceless"

Postby LarryLuke » Thu Apr 08, 2010 8:17 am

Case.........$600.00
Blue DVDs...$500.00
MB...........$400.00
CPU..........$600.00
SSD HD......$800.00
MEM.........$400.00
H2O stuff...$500.00



F%^^&&* side door won't close.............."Priceless"

User avatar
omegastitch
Garden Hose Sharpshooter
Garden Hose Sharpshooter
Posts: 173
Joined: Sat Sep 12, 2009 11:08 am
Location: Tooele, UT
Contact:

Re: New DIY "Priceless"

Postby omegastitch » Fri Apr 09, 2010 4:13 pm

looks like you just have to reroute or shorten a few tubes and you would be fine.
omegastitch

If ignorance is bliss, please let me die unhappy.

newdigitalblue
Water Pistol Grunt
Water Pistol Grunt
Posts: 18
Joined: Sun Nov 08, 2009 4:22 am

Re: New DIY "Priceless"

Postby newdigitalblue » Mon Apr 26, 2010 9:40 am

Did you put at RAD on the side door?
CASE: Corsair Obsidian Series 800D
CPU: Intel Core i7-920 Bloomfield
MOBO: EVGA E758-A1 3-Way SLI
RAM: G.SKILL 6GB (3 x 2GB)
GFX: EVGA GeForce GTX 285 1GB 512-bit DDR3 X1
PSU: KINGWIN Mach 1 1000W

LarryLuke
Water Pistol Grunt
Water Pistol Grunt
Posts: 4
Joined: Fri May 08, 2009 1:42 pm

Re: New DIY "Priceless"

Postby LarryLuke » Wed Sep 22, 2010 9:57 am

Hoses are not the problem.

The problem was the Coolance video card block. It has the hose attachments sticking way out to the side (like a hum on a camel's back). If they would have put the hose attachements somewhere in the middle of the block using 90 degree angles it would have been perfect.

Final solution was to completely remove the 480MM fan from the side (on top of the large radiator). I found it was not neccessary. The small 120MM fan at th rear of the case draws enough air through the side radiator to do the job. More quiet as well.


Return to “DIY and Modding”

Who is online

Users browsing this forum: No registered users and 2 guests