Another 1366 Build

Do-it-yourself and user modifications...
User avatar
Fluxc0re
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 96
Joined: Sat Dec 31, 2011 11:34 am
Location: Edmonton,Alberta
Contact:

Another 1366 Build

Postby Fluxc0re » Sun Apr 28, 2013 5:51 pm

Mark-up.jpg
(251.71 KiB) Not downloaded yet


A i7 920 with something to do . Aprox. Cost 1400.00 CDN

Xeon e5530 1366 Quad-core with a Koolance CPU-380I to keep it cool
6 Gigs Corsair Water-cooled RAM
EVGA 131-GT-E767-RX MotherBoard with A Swiftec Water-cooler on the Northbridge .
Koolance RP-1005 Pump and Rez .
2 inline temp sensors one on CPU one on RAM/Northbridge
2 Koolance SPL-XFR3 headers so it is easy to take off more lines to cool Videocards if you want to .
1 INS-FM17N Flowmeter .
1000W Coolermaster SilentPro PS .
1 ThermalTake MAC-3543 Hard Drive rack , 4 cages .
2 unmatched GTX-570s They work just fine in SLI .
1 unknown 240 3x thick rad with 2 , 3 speed fans on it . It had a leak but I fixed it .One of the fins got punctured by a fan screw but I sealed it up with epoxy and it has not been a problem since .

HardWare Count :
1 x CPU-380i "Refurb"
1 x Swiftec MCP-40 NorthBridge Cooler
1 X EK Ram Cooler
22 x Hose Connectors , compression and barb .
2 x SPL-XFR3 3-Way Swiveling Headers
1 x INS-FM17N FlowMeter
1 x RP-1005 Rez and Pump .
8' of 3/8 hose
18" of 1/2" hose
5 x 45* swiveling fittings
3 x 90* swiveling fittings
1 x 240 Rad 3X thick

P4290036_resize.JPG
(164.37 KiB) Not downloaded yet


P4290035 - Copy_resize.JPG
(96.88 KiB) Not downloaded yet


P4290032_resize.JPG
(241.68 KiB) Not downloaded yet
Last edited by Fluxc0re on Sun May 05, 2013 5:35 pm, edited 1 time in total.
i7950,EX21050,INSFM17N,SENAP008BP,CTRCD12,CPU360,GTX570,GTX560,6x1Gig,AX860i,
ThermaltakeMax2533,EVGAClassified141GTE770,FilterandRez.3.7LpmDCN "Einstein@home"
i7-920,RP-1005,ATI5770,12 Gigs of Kingston,Rad.Swifteck MCR-320.BF3 Box

User avatar
Fluxc0re
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 96
Joined: Sat Dec 31, 2011 11:34 am
Location: Edmonton,Alberta
Contact:

Re: Another i7 920 Build

Postby Fluxc0re » Thu May 02, 2013 9:10 pm

Well I just traded off the 920 and put in a e5530 Xeon in in its place .
Not a big performance hit as far as I can see and it runs cooler at stock .
I OCed it to 2.88 and now it runs at 55*c at 100% 8 threads E@Home after 8+ hrs .
Changes : Took apart that EVGA 570 and put on a GPU-200 .
It now runs at 36* C running 2 tasks for E@Home ,With the RP-1005 pump set to 5 .

P5040049.JPG
(72.89 KiB) Not downloaded yet
i7950,EX21050,INSFM17N,SENAP008BP,CTRCD12,CPU360,GTX570,GTX560,6x1Gig,AX860i,
ThermaltakeMax2533,EVGAClassified141GTE770,FilterandRez.3.7LpmDCN "Einstein@home"
i7-920,RP-1005,ATI5770,12 Gigs of Kingston,Rad.Swifteck MCR-320.BF3 Box


Return to “DIY and Modding”

Who is online

Users browsing this forum: No registered users and 1 guest