ASUS RoG Maximus VI Formula and my first water cooled PC

Do-it-yourself and user modifications...
Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio

Re: ASUS RoG Maximus VI Formula and my first water cooled PC

Postby Ace0751 » Sat Sep 07, 2013 2:54 pm

I was just going to sign on and say something along these lines lol. If you would like to still use the sensors then look into the TMS board mentioned earlier it holds up to 4 sensors and can do a lot more than just that and if you want you could add the attachment board later for more extra features. I think this is a better route to take than buying all this stuff and having wires going everywhere. At least with the TMS all you need to plug in for power is a 4 pin connector and it gives you all of your readings with their downloadable program. And I agree with IZ with using the software to monitor your temps I believe Nvidia has something with their program to monitor the temps of their cars and I use CoreTemp to monitor the CPU temps. I don't know a lot about that motherboard but I believe those are sensors that monitor certain parts of the board and you will be able to see them in the bios and the programs.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case


Return to “DIY and Modding”

Who is online

Users browsing this forum: No registered users and 2 guests