Customer Case Gallery

Complete water cooling systems (for example: Exos-2.5, PC5-1336, etc.)...

Customer Case Gallery

Postby sniperbob » Mon Sep 22, 2008 1:00 pm

Seeing as there is nothing in this topic, and most cases fall under this category, I figured I would start the CASE GALLERY!

Post your custom modded cases featuring Koolance Gear. Show us what you got and what you can MOD!

Please try to keep pictures of an adequate size and to post an adequate number of pictures. Too many per poster can really clog up the thread.

I suppose I'll start:

Koolance PC2-901BW Server Tower

Old Setup
Image

New Block!
Image

Second Rad!
Image


This is a more in depth build log:
http://www.xtremesystems.org/forums/showthread.php?t=194908
TOWER
Koolance PC2-901BW Server Tower
ASUS M2N SLI Deluxe
AMD Athlon 64 x2 5400+ BE (3.2 Ghz OCed)
PNY 9800GTX+
WD Caviar 160GB
WD RAPTOR 74GB
Koolance CPU-340 with MCP-655, MCR-220, MicroRes, and Tygon 1/2ID-3/4OD R3400 Tubing
sniperbob
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 14
Joined: Mon Sep 22, 2008 11:46 am

Re: CASE GALLERY

Postby [Koolance] Dean » Mon Sep 22, 2008 1:31 pm

Very nice, I saw that build log a couple days ago and especially liked the packard in the background =P.

this is my previous system working a new one now though.
Image
Image

not a very heavy duty mod but I'm pretty proud of the CPU lighting
[Koolance] Dean
 

Re: CASE GALLERY

Postby jad3f1r3 » Tue Sep 23, 2008 7:40 am

Here is my System! Lian Li Case Older PC-75B with Koolance Drop in Kit. Koolance cpu-340 on my E8400 oc to 4.8. The video card is an EVGA 9800 GX2 with EK Water Block, this is on the koolance loop green liquid. The Motherboard is an Asus Stiker 2 Formula with EK Water Blocks on a separate system than the cpu and gpu, and is blue liquid.
Attachments
P1050598sm.JPG
(46.73 KiB) Downloaded 303 times
User avatar
jad3f1r3
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 2
Joined: Tue Sep 23, 2008 7:35 am

Re: CASE GALLERY

Postby gotcow? » Tue Sep 23, 2008 9:32 pm

jad3f1r3 wrote:Here is my System! Lian Li Case Older PC-75B with Koolance Drop in Kit. Koolance cpu-340 on my E8400 oc to 4.8. The video card is an EVGA 9800 GX2 with EK Water Block, this is on the koolance loop green liquid. The Motherboard is an Asus Stiker 2 Formula with EK Water Blocks on a separate system than the cpu and gpu, and is blue liquid.


Upload a bigger picture chief.
Image
User avatar
gotcow?
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 23
Joined: Thu Sep 18, 2008 12:50 pm
Location: Pennsylvania

Re: CASE GALLERY

Postby Superman » Mon Sep 29, 2008 3:45 pm

http://overclockaholics.com
Silverstone TJ10esa
Evga 790i Ultra
Zues 1200w
Qx9770 4.8ghz
OCZ 2000mhz 2gb
Evga 9800gx2 QuadSLO
Creative X-Fi Fatality
Areca 1220 X6 150gb Raptor Raid 0(XpPro/Xp64/VistaU32/VistaU64 QuadBoot)
LG Multi Format/writer
Mitsumi FDD
30" Apple Cinema Display
24"Samsung
Logitech 5.1 Surround
25335 3dmark06 http://service.futuremark.com/compare?3dm06=6918656
http://overclockaholics.com
Last edited by Superman on Mon Nov 09, 2009 10:45 pm, edited 1 time in total.
Doomsday Rig:
TJ10ESA 1200w Zeus
Evga 790i Ultra SLI
Qx6700,6850,9650,9770 4.4ghz-5.4ghz
OCZ 9-9-9-28 1.8v 2000mhz 2x1gb
Evga 9800gx2X2
BFG Ultra OC X2
150gb RaptorX6
Areca 1220 Raid 0
Xonar X2
QuadBoot xp'z-VistaUlt'z
Overclockaholics.com/forums
Image
User avatar
Superman
Water Balloon Grenadier
Water Balloon Grenadier
 
Posts: 64
Joined: Mon Sep 29, 2008 3:30 pm
Location: Krypton, Hawaii

Re: CASE GALLERY

Postby TwinDragon » Fri Oct 17, 2008 12:26 am

I have a few builds so ill just link each seprate build.

qx6700
2 8800gtxes
Striker Extream
http://i219.photobucket.com/albums/cc17 ... 0_2202.jpg
http://i219.photobucket.com/albums/cc17 ... 0_2212.jpg

qx6700
1 soon to be 2 8800gtxes
Bx2 mobo soon to be striker II formula
Truhopes case
http://i219.photobucket.com/albums/cc17 ... 0_2214.jpg
http://i219.photobucket.com/albums/cc17 ... ights2.jpg
http://s219.photobucket.com/albums/cc17 ... 324292.pbw
more modding to do

here is this first beast that got me in to koolance lol the huge EYE SORE
e6600
xbx2
8800gtx
http://i219.photobucket.com/albums/cc17 ... 7Large.jpg
http://i219.photobucket.com/albums/cc17 ... 1Large.jpg
http://i219.photobucket.com/albums/cc17 ... 6Large.jpg
Told ya it was ugly!

NEw pc
qx6700
striker II formula
Tri 260gtxes
http://i219.photobucket.com/albums/cc17 ... 0_2342.jpg
http://i219.photobucket.com/albums/cc17 ... 0_2341.jpg
http://i219.photobucket.com/albums/cc17 ... 0_2340.jpg
http://i219.photobucket.com/albums/cc17 ... 0_2338.jpg
LOL the case was so heavy the bottom busting out :)

and yet again there will be 2 more new ones here in the next few months.
TwinDragon
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 13
Joined: Thu Oct 16, 2008 11:58 pm

Re: CASE GALLERY

Postby Izerous » Mon Oct 20, 2008 3:27 am

Image
These are not the best pictures, things are a bit dusty and messy. And the face plate for the hidden dvd-burner fell off. Haven't had time to re-attach it properly. The UV effects don't' show very well but there are 4 AC Ryan dual over boosts for the UV. And the window is a 2-way mirror so it prevents a crisp image.

Image
I took out the front plastic grill vent thingy. And replaced it with a a mesh. Inside i cut out some of the excess metal between the hard drives and the new fans. Completely removed the 80mm mountings in the hard drive cages, better airflow from the larger fans that way and due to the case's short depth and everything inside gave me a bit more clearance behind the hard drives from being able to move them forward. The 5.25 thing right above the x-fi breakout box is Sunbeam Light bus. Actually works pretty well for controlling everything that I typically have hooked up. The 4 buttons on in the 3.5 drive space. 2 are dvd-roms, and the other 2 controls ram led's. However moving to dominator ram i ditched them.

Image
Bottom rad in this picture is part of the KIT-1000 i purchased. The one that came with the enclosure and the mounting to mount it externally. Top is the 1.2KW Koolance PSU.

Image
Trying to show that the ac ryan's are bright, they actually make the external hosing glow as well. It's Feser black UV and as mentioned before the camera doesn't pickup the UV all that well.

Image
There is a 30 led, led strip right below the window. There was 2x30red and 2x30green however had issues with the glue holding where i placed them so removed them for the time being.
Corsair 800D
PSU-1200
M3N-HT Deluxe
RP-1000 > AMD 955 (3.7Ghz) > 1.120 > 2x8800GTS SSC (650:1523:880) > 3.120 > return
8GB Ram
128GB SSD + 300GB 10K + 3TB 7.2K
Adobe ACE for Flex3/AIR
Izerous
Water Cannon Artilleryman
Water Cannon Artilleryman
 
Posts: 569
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: CASE GALLERY

Postby dmartin95 » Thu Oct 23, 2008 8:30 pm

Great looking Rigs you all have there!
dmartin95
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 2
Joined: Thu Oct 23, 2008 8:28 pm

Re: CASE GALLERY

Postby Naekuh » Wed Jan 07, 2009 12:20 pm

oh you guys want to see my rig. :twisted:

Here it was when i was messing with the 9800GX2
Image

Here is when i was messing with my HD4870X2
Image

i'll have one of xfire up soon.

I call this the uber koolance delivery system. (well it feeds my KL-350 only) :mrgreen:
Image

Heres the shot of the naked board without tubings or fittings:
Image
Naekuh
Water Pistol Grunt
Water Pistol Grunt
 
Posts: 8
Joined: Tue Jan 06, 2009 6:23 pm

Re: CASE GALLERY

Postby Team NexGen » Wed Jan 07, 2009 9:30 pm

Woot! I will post my Pix as soon as I can find them
"if it Dont OverClock its Broken!"
www.NexGenOverclocking.com
Team NexGen
Water Balloon Grenadier
Water Balloon Grenadier
 
Posts: 59
Joined: Mon Sep 22, 2008 1:28 pm
Location: North Idaho

Next

Return to Water Cooling Systems & Kits

Who is online

Users browsing this forum: Google [Bot] and 0 guests

cron