For Sale - Koolance 1200W Liquid-Cooled Power Supply

Buy, sell, or trade your Koolance gear...
Killabee
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sun Jan 24, 2010 4:49 am

For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby Killabee » Sun Jan 24, 2010 5:23 am

I have a USED Koolance 1200W Liquid-Cooled Power Supply

I paid $495.00 for this brand-new from Performance-pcs.com
Im asking $300.00 for mine.

I only used this for about 6 months before i deployed to Afghanistan. This PSU does exactly what it was designed to do. put out massive amounts of power. Im selling this PSU to help me get funds for another PSU that is compatible with my matrox triplehead2go box. There is nothing wrong with this PSU. I also have the original packaging and book that came with it. If you have any other questions please let me know. Also please note that this item has been discontinued by Koolance. I dont know why, so if you have any info on the reasons post that up as well.

Image
Image
Image



The patented Koolance PSU-1200ATX-12S features 96A (simultaneous 12V@85A) over four 12V rails, and 4 PCI-Express connectors for SLI™ and CrossFire support. It is able to unleash 1200W of continuous (1400W peak) power at greater than 80% efficiency by operating in a completely submerged state. This patent-pending design is superior to even "partly" water cooled and heatpipe power supplies. All internal electronics are immersed in a non-conductive fluid and dissipated through an external heat exchanger.

Being self-cooled, Koolance's 1200W PSU requires no connections to any other type of water cooling system. The unit comes pre-filled and no ongoing coolant maintenance is required. The quiet 120mm LED fan is temperature-controlled and operates between 25-33dBA. An included temperature sensor allows internal monitoring when used with compatible Koolance systems (TMS, RP-1000, PC3-700, Exos-2, and PC4-1000 series).

The PSU-1200ATX-12S can be used in most ATX, E-ATX, and BTX chassis that provide for 9" (23cm) power supply depths, including cable space. The external heat exchanger is highly adjustable to maximize chassis compatibility. Being slightly wider than the internal power supply, it can be rotated 180° and moved vertically 2" (5cm) to help avoid physical conflicts. Quick disconnect shutoff valves allow for the convenient attachment of the heat exchanger during installation.

NOTE: The PSU-1200ATX-12S will operate in two mounted directions (standard/upright and on its side). Please see the user manual for details.

Power Specifications

Type EPS12V
Max. Power 1200W Continuous, 1400W Peak (@ 40°C)
Operating Range 90-264 VAC, Auto Switching
Current 15A @ 115V
Fan Dual Ball-Bearing 120mm, 30-107CFM, 25-33dBA,
Temperature Adjusting
PFC Active
Efficiency >80%
Power Factor >0.9
DC Output


+5V @ 30A
+12V @ 96A (12V1@18A, 12V2@18A, 12V3@30A,
12V4@30A); total combined 12V max = 85A
-12V @ 0.8A
+3.3V @ 30A
+5VSB @ 3.0A
Regulation 3% (3.3V, +5V, +12V) +9-5% (-12V)
Ripple 1% (+5V, +5VSB, -12V), 1.5% (+3.3V), 2% (12V)
Hold Time 16ms min.
PG Delay 100~500ms
OV Protection +3.3V, +5V, +12V (all output to ground)
OC Protection +3.3V, +5V, +12V (all output to ground)
Temperature 0-40°C (for external heat exchanger only)
Humidity 20-90% RH
Certifications NVIDIA® SLI™ Ready
Connectors 1 x 24-pin motherboard
1 x 8-pin 12V CPU/motherboard
4 x (1-plug) PCI-E
2 x (3-plug) SATA
2 x (4-plug) Molex peripheral
1 x (4-plug + 1 FD) Molex peripheral + floppy


Unit Specifications
Model PSU-1200ATX-12S
Compatibility ATX, E-ATX< BTX
Materials Aluminum, Steel, Engineering Resin, Coolant Liquid
Tubing Size, ID 1/4", 6mm
Product Dimensions
WxHxD (PSU) 6" x 3.2" x 8.27" (15.2cm x 8.1cm x 21cm)
Product Dimensions
WxHxD (Heat Ex.) 6.8" x 5.6" x 4.1" (17.2cm x 14.1cm x 10.5cm)
Product Weight 13.6 pounds (6.2kg)
Warranty 2 years

Components Included
Power supply with external heat exchanger assembly, pre-filled coolant, AC power cable, 1 x 24-pin motherboard cable, 1 x 8-pin 12V CPU/motherboard cable, 4 x (1 plug) PCI-E cables, 2 x (3 plug) SATA cables, 2 x (4 plug) Molex cables, 1 x (4 plug, 1 FD) Molex + floppy power cable, temperature sensor cable, user manual

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby bambihunter » Wed Jan 27, 2010 10:44 am

So how old is it in total? Do you know the revision of it?
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby Izerous » Wed Jan 27, 2010 11:02 am

I believe the reason they discontinued the standalone versions are as follows.Unlike the newer ones it isn't as maintenance free. The quick disconnects are not the newer no spill ones so fluid is lost overtime when you take it in and out of cases, thus overtime you will need to eventually refill it. The fluid inside not being standard fluid is a bit more expensive. The new ones don't have this same issue as the fluid used to submerge the components are sealed, and the plate heat exchanger means none of it should be lost even over time.

I have had mine since they were first released (near Jan 2007 according to the product page) and I'm really close to needing to get my hands on some fluid to top it off. But I do take mine in and out of the case when doing mods etc. If longer periods between attaching and removing the back fluid will last longer.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

dumbeldor
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Thu Jan 28, 2010 3:55 am

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby dumbeldor » Thu Jan 28, 2010 4:04 am

hello,


Looks really good your liquid cooled power supply are in good condition and the rates that you fixed for it are also reasonable. so i will try to find any person if i get anyone then i will tell you about that.




thanks


____________
twin xl comforter

User avatar
HELLFIRETOYZ
Tactical Bucket Splasher
Tactical Bucket Splasher
Posts: 301
Joined: Sat Nov 01, 2008 8:56 pm
Location: Peoria, AZ
Contact:

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby HELLFIRETOYZ » Thu Jan 28, 2010 11:46 am

I had a customer inquire about the fluid a while back and I contacted Koolance about it. They informed me the fluid was more than the PSU was worth and would dissipate if exposed to air...
Hellfire - multi-mission, and multi-target precision-strike capability weapon system, "fire-and-forget!"

BFG GTX285 OC'd 3-Way Blocked
Asus P6T7 SuperComputer Blocked
i7 920 @ 4.21Ghz Blocked
Corsair DDR3 1600 - 6Gb
OCZ Vortex SSD 120

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby bambihunter » Thu Jan 28, 2010 10:18 pm

I would think it would be the same fluid they use in immersed transformers. You're right, the stuff isn't cheap, but it isn't THAT expensive. :o
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans

User avatar
HELLFIRETOYZ
Tactical Bucket Splasher
Tactical Bucket Splasher
Posts: 301
Joined: Sat Nov 01, 2008 8:56 pm
Location: Peoria, AZ
Contact:

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby HELLFIRETOYZ » Fri Jan 29, 2010 12:28 pm

$150 a bottle is what they said...not sure how big the bottle was.
Hellfire - multi-mission, and multi-target precision-strike capability weapon system, "fire-and-forget!"

BFG GTX285 OC'd 3-Way Blocked
Asus P6T7 SuperComputer Blocked
i7 920 @ 4.21Ghz Blocked
Corsair DDR3 1600 - 6Gb
OCZ Vortex SSD 120

Killabee
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sun Jan 24, 2010 4:49 am

Re: For Sale - Koolance 1200W Liquid-Cooled Power Supply

Postby Killabee » Mon Feb 08, 2010 5:27 am

the only time i have disconnected the hoses is during the install. Other than that there has been no fluid discharged from my PS. The reservoir is still full.


Return to “Buying / Selling / Trading”

Who is online

Users browsing this forum: No registered users and 1 guest