TMS-200 (Software v2.1.28 *Beta*) Feedback - Post Here

Koolance TMS Software & Hardware Interface...

Does this software version stop your alarm-at-bootup? (Vote changing is allowed.)

Poll ended at Fri Jan 14, 2011 9:48 am

Yes
3
50%
Sometimes
2
33%
Not at All
1
17%
 
Total votes: 6

santiagodraco
Water Pistol Grunt
Water Pistol Grunt
Posts: 9
Joined: Fri Sep 19, 2008 4:25 pm

Re: TMS-200 (Software v2.1.28) Feedback - Post Here

Postby santiagodraco » Wed Nov 24, 2010 10:11 am

This only resolves the issue 50% of the time for me.

Whatever is causing the problem appears to be related to the boot process and once it boots successfully then the next time that boot process has caused the problem to reappear. Since I'm not opening and resaving settings this means that there will be a beep on the next boot.

I'd suggest that the software resave settings ever time it's successfully starts up and communicates with the device. Assuming that it's when it saves changes to the card that the problem is being resolved that is. This way when the problem reappears (and it does) this might keep it from reappearing.

So no, this version is definitely not a 100% fix.

User avatar
Balthazor
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 56
Joined: Wed Jan 06, 2010 3:37 am

Re: TMS-200 (Software v2.1.28) Feedback - Post Here

Postby Balthazor » Tue Nov 30, 2010 2:59 am

"•Added some improvements that may decrease COM connection time on slower systems."

I have one of the fastest combinations of current hardware, and even so I noticed a dramatic decrease of COM connection times. So good job on that aspect of this update.
Koolance TMS-200 / RP-1000 / EHX-1320 w/ HBK Fans / TT TMG-1 120mm Rad w/ Koolance HBK Fan / CPU-360 v1.1 / VID-597 v2 / EK Chipset Water block
Gigabyte x58a-UD7 / 980-x / 12GB RAM / 2 x HD5970
Creative X-Fi Titanium / Killer 2100 / Windows 7 x64

User avatar
Admin
Moderator
Moderator
Posts: 126
Joined: Tue Sep 09, 2008 5:36 pm
Location: WA, USA

Re: TMS-200 (Software v2.1.28 *Beta*) Feedback - Post Here

Postby Admin » Mon Dec 20, 2010 2:59 pm

For customers now using software version 2.1.28 *Final*, please continue discussion at viewtopic.php?f=21&t=1900


Return to “Software”

Who is online

Users browsing this forum: No registered users and 1 guest