tms 205 software newest version

Koolance TMS Software & Hardware Interface...
Mikesnow
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 76
Joined: Sun Jul 19, 2009 11:39 pm
Contact:

Re: tms 205 software newest version

Postby Mikesnow » Sat Jun 08, 2013 3:34 am

I like it better then the old software for the fan adjustments, hoping you add the c/f change setting. the other software interface was graphically more pleasing as well, but het i'd rather have functionality over looks myself.
Asus Rampage IV Extreme
Intel Core I7-3930K w/CPU-360
32GB Patriot Viper3 Series 2133MHz Ram
2x Corsair Performance Pro CSSD-P256GBP-BK (Raid0)
2x Western Digital - 1TB HDD (Raid1)
EVGA GTX 680 w/VID-NX680
Silverstone ST1500 PSU
Corsair Obsidian 800D

Mikesnow
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 76
Joined: Sun Jul 19, 2009 11:39 pm
Contact:

Re: tms 205 software newest version

Postby Mikesnow » Thu Jun 13, 2013 5:18 pm

Finally got all my stuffs in and got my system together last night. Couldn't ever get the beta version to work, it would never connect to my tms-200. Installed the older 2.1.30 and it found the board and works. Restarted the beta 3.0 and it connected, apparently something is missing from the installer on the beta that's needed by the tms-200. Started up the system from cold boot just now and got a .net error message. Guess I'll leave it here in case it helps you guys in any way.

Code: Select all


See the end of this message for details on invoking
just-in-time (JIT) debugging instead of this dialog box.

************** Exception Text **************
System.Runtime.InteropServices.ExternalException (0x80004005): A generic error occurred in GDI+.
   at System.Drawing.Graphics.Clear(Color color)
   at WinFrmsApp.main1.uGrapDrawing(Boolean change) in C:\Documents and Settings\dhkim\바탕 화면\TMS205\C#4\source\TMS205Light\TMS205Light\TMS205Light\main1.cs:line 1205
   at WinFrmsApp.main1.timeGraph_Tick(Object sender, EventArgs e) in C:\Documents and Settings\dhkim\바탕 화면\TMS205\C#4\source\TMS205Light\TMS205Light\TMS205Light\main1.cs:line 1174
   at System.Windows.Forms.Timer.OnTick(EventArgs e)
   at System.Windows.Forms.Timer.TimerNativeWindow.WndProc(Message& m)
   at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)


************** Loaded Assemblies **************
mscorlib
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.296 (RTMGDR.030319-2900)
    CodeBase: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
----------------------------------------
TMS205Beta
    Assembly Version: 1.0.0.0
    Win32 Version: 3.0.0.0
    CodeBase: file:///C:/Program%20Files%20(x86)/Koolance/TMS%20205%20Light%20v3.0.0%20Beta/TMS205Beta.exe
----------------------------------------
System
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.1001 built by: RTMGDR
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Windows.Forms
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.1002 built by: RTMGDR
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System.Drawing
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.1001 built by: RTMGDR
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
System.Configuration
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.1 (RTMRel.030319-0100)
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
----------------------------------------
System.Xml
    Assembly Version: 4.0.0.0
    Win32 Version: 4.0.30319.233 built by: RTMGDR
    CodeBase: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
----------------------------------------
xCtlProgressBars
    Assembly Version: 1.0.0.0
    Win32 Version: 1.0.0.0
    CodeBase: file:///C:/Program%20Files%20(x86)/Koolance/TMS%20205%20Light%20v3.0.0%20Beta/xCtlProgressBars.DLL
----------------------------------------

************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.

For example:

<configuration>
    <system.windows.forms jitDebugging="true" />
</configuration>

When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.

Asus Rampage IV Extreme
Intel Core I7-3930K w/CPU-360
32GB Patriot Viper3 Series 2133MHz Ram
2x Corsair Performance Pro CSSD-P256GBP-BK (Raid0)
2x Western Digital - 1TB HDD (Raid1)
EVGA GTX 680 w/VID-NX680
Silverstone ST1500 PSU
Corsair Obsidian 800D

FuzzDad
Water Pistol Grunt
Water Pistol Grunt
Posts: 4
Joined: Sun Apr 10, 2011 1:15 pm
Contact:

Re: tms 205 software newest version

Postby FuzzDad » Sun Jun 16, 2013 9:24 am

I've found on my PC that if I power off the machine I need to re-install the profile driver and the software in a specific sequence to get it to work (turn off software, pull usb cable out of TMS-200, re-install the profile driver, reboot, put cable back in, restart the software)...but when it works it works fine in both x64 win7 and win 8. I like the minimalist approach a lot.

Issues/Desires (other than power-off deal that may be related to my mobo...not the software)

1) I'm not using a few of my fan ports but it still states "100%" on in the block even though there's no fan in use for that port. That's not consistent with how you display the pumps or flow meter when they are not being used (you show nothing if those are not installed).
2) I would like the gallon or liter choice back.
3) Would be nice if you could read the bios to get at CPU and MB temps...I run other utilities for those but it would be nice to have them all in one app.

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA
Contact:

Re: tms 205 software newest version

Postby [Koolance] Tim » Tue Jun 18, 2013 9:01 am

Our programmers have confirmed the software should be compatible with TMS-200. The only real difference between it and TMS-205 is the temperature sensor value. They are investigating the issues being posted here.

°C/°F and LPM/GPM toggle options are also being added.

Mikesnow
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 76
Joined: Sun Jul 19, 2009 11:39 pm
Contact:

Re: tms 205 software newest version

Postby Mikesnow » Tue Jun 18, 2013 5:58 pm

That code I posted I get rather often. Also, this is a bit nit picky, but if it were me I would make the status bar for the temps go under the names for them so like;

Temp1
------------
Temp2
------------

That way you can name your temp sensors more then just a few letters, but the looks are still nice looking.
Asus Rampage IV Extreme
Intel Core I7-3930K w/CPU-360
32GB Patriot Viper3 Series 2133MHz Ram
2x Corsair Performance Pro CSSD-P256GBP-BK (Raid0)
2x Western Digital - 1TB HDD (Raid1)
EVGA GTX 680 w/VID-NX680
Silverstone ST1500 PSU
Corsair Obsidian 800D

Montegobei
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Jul 23, 2013 4:02 pm
Contact:

Re: tms 205 software newest version

Postby Montegobei » Tue Jul 23, 2013 4:29 pm

Hi Tim,
I have TMS-205 and extension board setup connected with 2 PMP-450 pumps. Problem is I can't control pump speed. Software just shows rpm what is set on the pump manually. Everything else connected works very well (4 fans, 1 flow meter, 10 temp sensors).
I tried to disconnect one pump and control just one pump, tried to switch the pump connectors, reinstalled software...nothing helped. Any tips?
Thank You

PS: I have Windows 8. Attached is picture you could check
Attachments
Desktop_2013_07_23_19_26_39_217.jpg
software pic
(254.65 KiB) Not downloaded yet

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio
Contact:

Re: tms 205 software newest version

Postby Ace0751 » Wed Jul 24, 2013 4:40 pm

If you have the 450 and not the 450s the pump speed are on top of the pumps that's how you control them.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case

Montegobei
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Jul 23, 2013 4:02 pm
Contact:

Re: tms 205 software newest version

Postby Montegobei » Wed Jul 24, 2013 5:01 pm

I know... Problem is I need to control speeds in the software interface not manually, that's the idea:)

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio
Contact:

Re: tms 205 software newest version

Postby Ace0751 » Wed Jul 24, 2013 5:18 pm

Ah just making sure, but that would be a great feature to have though especially with my case its a major pain to change the speed manually since its all acrylic lol.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case

Mikesnow
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 76
Joined: Sun Jul 19, 2009 11:39 pm
Contact:

Re: tms 205 software newest version

Postby Mikesnow » Thu Aug 01, 2013 1:43 am

Any idea on when theres an updated version? These little error messages are getting annoying they always poping up when I start up programs.
Asus Rampage IV Extreme
Intel Core I7-3930K w/CPU-360
32GB Patriot Viper3 Series 2133MHz Ram
2x Corsair Performance Pro CSSD-P256GBP-BK (Raid0)
2x Western Digital - 1TB HDD (Raid1)
EVGA GTX 680 w/VID-NX680
Silverstone ST1500 PSU
Corsair Obsidian 800D


Return to “Software”

Who is online

Users browsing this forum: No registered users and 1 guest