TMS-200 + Expansion - How many fans can I expect to manage?

Koolance TMS Software & Hardware Interface...
rgeneson
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Mon Aug 24, 2009 9:57 pm

TMS-200 + Expansion - How many fans can I expect to manage?

Postby rgeneson » Mon Aug 24, 2009 10:28 pm

I'm looking at purchasing a TMS-200 w/expansion to control a double-loop set-up with two 120X3 radiators. I notice the maximum amperage for the board is listed at 6.5, does the expansion board expand this limit? Has anyone had any luck with multiple sets of daisy chained fans (say two or even three 4-fan wiring harnesses connected to a single TMS-200)? Also, what is the maximum Watts value for the TMS200 + expansion board, would it be on the order of 78 (6.5 amps X 12 Volts)? I'm building out a Mountain-Mods Ascension so I've got a LOT of fans I could possibly control and I'm trying to understand what the upper limit is. My fans draw between .40 and .74 amps.

User avatar
[Koolance] Tim
Moderator
Moderator
Posts: 451
Joined: Tue Sep 16, 2008 9:34 am
Location: WA, USA

Re: TMS-200 + Expansion - How many fans can I expect to manage?

Postby [Koolance] Tim » Thu Aug 27, 2009 3:38 pm

6.5A is the TMS' Molex connector limit. The expansion board could not allow for a higher consumption since it shares power through the main board.

astrodanco
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 59
Joined: Wed Jul 01, 2009 7:10 pm
Location: San Diego, CA

Re: TMS-200 + Expansion - How many fans can I expect to manage?

Postby astrodanco » Thu Aug 27, 2009 7:27 pm

This is the response I received from Koolance technical support:

We do not recommend higher than 2 amps per fan header and 3 amps per pump header. The maximum voltage is always 12v so 24w and 36w are the maximum draw respectively.


They should have added the 6.5A caveat for the whole main plus expansion board like you did.
Core i7 920 (D0) @ 4.0Ghz, P6T Deluxe V2 (1003), 12GB CM3X2G1600C7 @ 1600 7.7.7.20 2T, ATCS 840, Antec TPQ 850, Radeon 4850, TMS-200+EB200+FM17, EK Supreme HF, EK-D5 dual top, 2X MCP-655-B, MCR-320, 6X Skythe D1225C12B5AP-15, Durelene tubing, BP fittings.

rgeneson
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Mon Aug 24, 2009 9:57 pm

Re: TMS-200 + Expansion - How many fans can I expect to manage?

Postby rgeneson » Fri Aug 28, 2009 11:36 am

Excellent information -- thank you very much!

Ryan


Return to “Software”

Who is online

Users browsing this forum: Google Feedfetcher and 1 guest