F*** my laptop

Post your speeds and temps, or just talk shop.
newdigitalblue
Water Pistol Grunt
Water Pistol Grunt
Posts: 18
Joined: Sun Nov 08, 2009 4:22 am

F*** my laptop

Postby newdigitalblue » Mon Apr 26, 2010 9:37 am

So here I am in lovely Florida just got my laptop back after an RMA for faulty fans which I only discovered after I discovered it was running hot with low performance. So the fans are working but the laptop still isn't performing up to specs. I'm about to throw a lot out there. but here is what I'm reading off of pcwizard. At a very low load C1: 3% and C2:6% (installing steam after a fresh install of windows 7 and running yahoo messanger and mozilla Firefox only) my CPU temp is 80C with my GFX temp is at 44C with of course no load on it. What do?

General Information :
Real Frequency : 1595.45 MHz
Multiplier : 8x
Low/High Multiplier : 6x / 13x
IDA ratio : 14x
Multiplier Locked : Yes
Marketing Frequency : 2600 MHz
Intel Dynamic Acceleration : 2800 MHz

Front Side Bus Information :
Bus Speed : 199.4 MHz
FSB Frequency : 797.7 MHz (QDR)
Turbo Mode : No
LFM Frequency : No
C0 State : Yes

Initial Frequencies :
Frequency : 2600 MHz
Bus Speed : 200.00 MHz (QDR)
Multiplier : 13x

Frequency Control :
Core #1 : 1595.56 MHz
Core #2 : 1595.52 MHz

Control Clock Frequency :
Enhanced SpeedStep (EIST) : Yes - Enabled
C1E - Enhanced Halt Mode : No
Dynamic FSB : Yes - Enabled
Dynamic Acceleration (IDA) : Yes - Disabled
Turbo Mode : No

Thermal Information :
Thermal Design Power : 65 W
Thermal control TM1 : Yes - Disabled
Thermal control TM2 : Yes - Disabled
Thermal Control Circuit : No
Digital Thermal Sensor : Yes
Clock Modulation (ODCM) En... No

General Information :
Type : Intel Mobile Core 2 Duo
Internal Specification : Intel(R) Core(TM)2 Duo CPU T9500 @ 2.60GHz
Model Number : T9500
Codename : Penryn
Revision : C0
Technology : 0.045µ
CPU ID : 6.7.6
CPU IDEx : 6.17.6
Microcode : MU06760C
Number of Physical Processors : 1
Mobile : Yes
CASE: Corsair Obsidian Series 800D
CPU: Intel Core i7-920 Bloomfield
MOBO: EVGA E758-A1 3-Way SLI
RAM: G.SKILL 6GB (3 x 2GB)
GFX: EVGA GeForce GTX 285 1GB 512-bit DDR3 X1
PSU: KINGWIN Mach 1 1000W

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: F*** my laptop

Postby bambihunter » Mon Apr 26, 2010 12:53 pm

Well, it looks like it is throttling back. This may be due to the power settings, or it could be thermal. That is really hot for idle. I'd send it back and tell the fk'ers to fix it right or replace it...
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans


Return to “Hardware and Overclocking”

Who is online

Users browsing this forum: No registered users and 1 guest