CPU-360 on LGA 2011

CPU water cooling blocks...
Speedway
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sun Feb 16, 2014 11:53 am

CPU-360 on LGA 2011

Postby Speedway » Sun Feb 16, 2014 12:09 pm

I am thinking about upgrading from the 2600K on LGA 1155 to the 3930K on the LGA 2011 platform. I didn't have any issues going from 1366 to 1155, but I am wondering if my CPU-360 will have any installation issues on an LGA 2011 mobo or cpu? Has anyone used a CPU-360 on 2011? If so did you have to do any modding or does the block fit without any issues? Any and all help would be greatly appreciated and thanks in advance.

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio

Re: CPU-360 on LGA 2011

Postby Ace0751 » Mon Feb 17, 2014 7:32 pm

May want to contact Koolance I believe the 360 is only made up to LGA 1366 but they have post screws that are compatible for the 360 that will fit on the 2011 boards. Best to contact them first, if you don't want to go through that hassle the 380 is a well deserved upgrade.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case

Speedway
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Sun Feb 16, 2014 11:53 am

Re: CPU-360 on LGA 2011

Postby Speedway » Tue Feb 18, 2014 2:51 am

Thanks for the reply. The 360 has been working great on my 2600K on the 1155 platform. When I went from 1366 to 1155, I didn't run into any issues. I was just wondering if anyone had used the 360 on the 2011 platform, notably the 3930K? Does the block cover the chip well and was the mount an easy fit or is there additional hardware needed.

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: CPU-360 on LGA 2011

Postby Izerous » Tue Feb 18, 2014 9:14 am

Browsing through accessories etc on the website I did come across this.

LGA-2011 Mounting Posts for CPU-360/370

Based on this product it looks like if you have a fixed back plate on the 2011 board you just need this screw set to make it work. I would still contact Koolance directly as Ace suggested to make sure that is all you need.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram


Return to “Water Blocks - CPU”

Who is online

Users browsing this forum: Google [Bot] and 1 guest