Dual-SLI GTX 680 cooling system questions

Video card/GPU water cooling blocks...
SpacemanSpliff
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Sat Apr 20, 2013 6:44 pm

Dual-SLI GTX 680 cooling system questions

Postby SpacemanSpliff » Sat Apr 20, 2013 7:20 pm

I'm planning on doing a new gaming only build towards the end of this year, so I figure it's always good to plan things in advance. I already know what components I want to use, but I'm debating with myself about whether or not I should set up a liquid cooling system to provide high performance cooling to the dual GTX-680 SLI configuration I want to use.

So far, this is the component list I have in mind:

AZZA Genesis 9000 tower
Gigabyte GA-Z77x-UD5H motherboard
Intel Core i7-3770K
G-Skill Trident X DDR3-2400 32GB memory
2x EVGA Superclocked Signature 2 2GB GTX-680s
LEPA 1000W G-Series 80+ gold cert. PSU
2x Kingston Hyper-X 240GB SSD in RAID-0
4x WD Caviar Black 1TB HDD in RAID-1

I plan on using a Cooler Master Seidon 240M or a Corsair H100i to cool the CPU on the bottom mount rails, which would free up the top mounts of the case to use a 480mm radiator setup to run a cooling system for the GPUs. Any thoughts or advice on how to build a GPU cooling system and/or any components alternatives that would be better suited for what I want to build is greatly appreciated as this would be my first time making a GPU cooling system. 8-)

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: Dual-SLI GTX 680 cooling system questions

Postby Izerous » Tue Apr 23, 2013 8:43 am

I'll be honest if your going to rig up the GPU's to a dedicated custom loop, toss the idea of the H100 etc out of your head and do the whole system. While the H100's and other units are not bad they don't compete with a full system, and the cost of a dedicated GPU loop + H100i comparing to adding the CPU to your GPU loop your thinking of is pretty small.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

User avatar
Fluxc0re
Water Balloon Grenadier
Water Balloon Grenadier
Posts: 96
Joined: Sat Dec 31, 2011 11:34 am
Location: Edmonton,Alberta

Re: Dual-SLI GTX 680 cooling system questions

Postby Fluxc0re » Sun Apr 28, 2013 4:46 pm

Well , to start with you need to get videocards that you can get waterblocks for .
And a boot drive that is SSD will help.
A motherboard that you can put waterblocks on the power section is a good thing .
A pump and rez combo like the RP-1200 and fittings .
i7950,EX21050,INSFM17N,SENAP008BP,CTRCD12,CPU360,GTX570,GTX560,6x1Gig,AX860i,
ThermaltakeMax2533,EVGAClassified141GTE770,FilterandRez.3.7LpmDCN "Einstein@home"
i7-920,RP-1005,ATI5770,12 Gigs of Kingston,Rad.Swifteck MCR-320.BF3 Box


Return to “Water Blocks - Video”

Who is online

Users browsing this forum: Bing [Bot] and 1 guest