Mounting in a 900D

Pumps and reservoirs
pologoalie8908
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Mon Nov 17, 2014 11:55 am
Contact:

Mounting in a 900D

Postby pologoalie8908 » Mon Nov 17, 2014 11:59 am

I need help/advice on how to mount my 80x240mm Reservoir in my 900D. My pump is in this [http://koolance.com/pump-nozzle-and-reservoir-base-for-pmp-450-60mm-od] base which the Reservoir is attached. The base comes with the adjustable mounting brackets but I am unsure how to mount it in my case. Any advice would be helpful. I don't want to have to drill into my case.

Izerous
Rain Maker
Rain Maker
Posts: 1183
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada
Contact:

Re: Mounting in a 900D

Postby Izerous » Tue Nov 18, 2014 9:02 am

A larger res doesn't actually help with anything except visuals and the bleeding process. Its negligible on cooling performance etc. If you don't want to make holes etc and cannot seem to find room for the 240mm res body I'd honestly suggest just getting a smaller body something like 80mm tall.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

pologoalie8908
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Mon Nov 17, 2014 11:55 am
Contact:

Re: Mounting in a 900D

Postby pologoalie8908 » Tue Nov 18, 2014 9:55 am

I have room for it im just wondering how to go about mounting it in the case. Ive seen people mount it to one of the hard drive cages using the adjustable mounts that come with the pump/res base combo

Pianosdr
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Dec 09, 2014 9:59 am
Contact:

Re: Mounting in a 900D

Postby Pianosdr » Tue Dec 09, 2014 10:52 am

I just mounted an 80mm res to my 900d last night. I mounted it to the drive cages on the right side, but this requires installing the drive cage to the middle area in order to have the screw holes for proper positioning. You'll also need to buy some small washers, spacers, and nuts.

Once you have the cages installed, then you use four long screws + spacers together and screw the reservoir bracket into that. Not all four of the bracket holes will line up with a hole on the drive cages though, so you will need to place screws wherever there are holes, and where there aren't, there'll at least be an opening that leads into the drive cage. With this, you'll need to put the screw through the bracket, through the spacer, and then into the drive cage opening. On the other side of the screw, you then put a washer + the nut around the screw and tighten. This will hold the screws in place and allow you to mount everything properly without having to make any new holes. However, the space for tightening the nut on the inside of the drive cage is pretty difficult to do, especially if you have a drive mounted to that sled (as I do), because you'll need to keep the sled in the cage while you screw everything in, as the screws will prevent the sled from coming out once installed. If you want to ever remove the sled later, you'll need to unscrew the reservoir bracket first.

So if you have a drive installed on the sled, then your hands will likely not be able to fit in there to hold the nut in place while you tighten. If this is your case (as it was mine), then you'll need to have some small grasping tool (like tweezers) in order to tighten. It's a fairly tedious process, so be prepared for a little frustration. Here are a couple pictures of what I'm talking about, taken from my case:

http://tinypic.com/r/140kke0/8
http://tinypic.com/r/f2sayh/8
http://tinypic.com/r/2ptp4c9/8


Return to “Pumps & Reservoirs”

Who is online

Users browsing this forum: No registered users and 2 guests