New Product suggestion!

Heat exchangers, fans...
JuanPabloCuervo
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 33
Joined: Sat Aug 01, 2009 8:42 am

New Product suggestion!

Postby JuanPabloCuervo » Mon Feb 21, 2011 6:08 pm

Hi...

i have the ERM-2k3u with rear fans dissabled/disconnected, works ok with 10 blocks.
in my PC also i have 2x120mm fans..
but i hate fans, what can i say....

the idea its to remove the 2x240mm fans & keep same temperatures or better...

the sollution would be to build something similar to an electric Tankless Water Heater...
but Cooler!

how?
just like Corsair ICE-T30 Sub ambient cooler... arround a 12mm id copper tube, that i can plug inline at the input or output of the ERM-2k3u..

http://www.youtube.com/watch?v=2zvLBzm4inw
http://en.wikipedia.org/wiki/Tankless_w ... ss_heaters

or... to install infront of the Radiators replacing the 2x240 fans.

also would be nice an smaller version to replace the 120mm fans inside my PC.

Thanks

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: New Product suggestion!

Postby Izerous » Mon Feb 21, 2011 11:30 pm

I don't really fully understand what your thinking but in short using TEC coolers doesn't instantly solve your problem. Electricity is one of the least efficient heat/cooling methods possible. Using a TEC cooler as done in the first link actually creates more heat on the hot side then there was in the first place.

Say a component outputs 50W of heat, you put in a TEC coolers to cool it but the hot side outputs 75W of heat instead. You now have to remove 75W of heat instead of only 50W of heat. There are instances that they work however. You didn't really explain your idea very well and you should elaborate more on it, even if it is mspaint doodles.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

JuanPabloCuervo
Water Shotty Skirmisher
Water Shotty Skirmisher
Posts: 33
Joined: Sat Aug 01, 2009 8:42 am

Re: New Product suggestion!

Postby JuanPabloCuervo » Tue Feb 22, 2011 8:06 am

i think im gonna try to modify a portable ice maker... or a 12 Volt Car, Beverage, Thermoelectric, Travel Cooler, Chiller, or Can cooler.
http://en.wikipedia.org/wiki/Icemaker

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: New Product suggestion!

Postby Izerous » Tue Feb 22, 2011 1:41 pm

Re-reading what you have not that I'm more awake instead of just before going to bed I think your essentially trying to replicate a Coolit Boreas unit, but attempting to make it fanless. It just means it needs a massive passive heat sink instead of compact active heat sink. Fridges don't have fans on the back because of the massive size of their cooling.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

bambihunter
Water Cannon Artilleryman
Water Cannon Artilleryman
Posts: 560
Joined: Wed Oct 08, 2008 9:56 am
Location: Oklahoma City, Oklahoma

Re: New Product suggestion!

Postby bambihunter » Wed Mar 16, 2011 12:52 pm

Just go phase change and forget it. :mrgreen: :geek:
PC5-1336BK
PSU-1300ATX
2 VID-NX295S
2 RP-1000
RP-980
CPU-350AC
2 CHC-122
MVR-100
AMD 955BE, 6 250gb in RAID0, 8GB OCZ Flex 1200, 2 EVGA GTX295 FTW's. Loop 1: CPU & quad GPU's. Loop 2: PS to 120mm to NB/SB/Vreg's to dual 80mm rad/fans


Return to “Radiators & Fans”

Who is online

Users browsing this forum: Google [Bot] and 1 guest