CTR-CD12 + INS-FM17N + SEN-AP008PB. OK?

Heat exchangers, fans...
booya
Water Pistol Grunt
Water Pistol Grunt
Posts: 7
Joined: Thu Dec 01, 2011 6:54 pm
Location: 55.7517° N, 37.6178° E

CTR-CD12 + INS-FM17N + SEN-AP008PB. OK?

Postby booya » Thu Dec 01, 2011 7:18 pm

Hello, I want to install CTR-CD12 Fan Controller and connect to it one temp. sensor SEN-AP008PB or SEN-AP008G and one INS-FM17N Flow Meter.

Also I need to connect with this thing 9 fans (each 0.09A).

So I need to use three 4-Fan Wiring Harness.

After that, i think this controller will be able to change rpm of all 9 fans, based on temp. sensor readout (only one sensor). For example, if we will have T of water ~30C, it will be low rpm. The higher temp, the higher rpm at fans.

This that possible?

Thx.
Phobya Balancer 450 Black Nickel -> Iwaki RD-30 -> XSPC RayStorm -> EK-FB KIT RE4 LE -> Koolance MB-ASR4E -> 3 x EK-FC Titan (in series) -> 2 x Watercool MO-RA3 Pro 9x140mm | hoses 13/16 | QDCs Koolance VL3N

AgentX250
Water Pistol Grunt
Water Pistol Grunt
Posts: 21
Joined: Fri May 13, 2011 1:18 pm

Re: CTR-CD12 + INS-FM17N + SEN-AP008PB. OK?

Postby AgentX250 » Tue Dec 06, 2011 11:06 am

The math says you'd be ok since the fans would only being pulling .81 amps, I cant say whether the controller would work out how you expect but it would be able to handle the fans and the meters.
Mobo: evga 780i FTW
CPU: intel q9650 @ 3.42 @ 1.25 (stock voltage)
GFX: 3x evga GTX470 SLI
Ram: 4gb ocz pc2-8500 @ 760mhz
PSU: Enermax revolution 85+ 1050 watt
Hdd: 1tb hitachi C, 2x 1tb WD (main/backups)
Cooling: full coverage custom liquid cooling

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: CTR-CD12 + INS-FM17N + SEN-AP008PB. OK?

Postby Izerous » Tue Dec 06, 2011 12:21 pm

I would double check your fan's specs (0.09A) but yes as Agent mentioned you should be ok.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram


Return to “Radiators & Fans”

Who is online

Users browsing this forum: No registered users and 2 guests