Need help with 452 1.3v drivebay res.

Pumps and reservoirs
v3teran
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Tue Jul 15, 2014 6:31 pm
Contact:

Need help with 452 1.3v drivebay res.

Postby v3teran » Wed Jul 16, 2014 12:16 pm

Im finding it hard to bleed all the air out of this, whenever i watch the bubbles come back around into the res they instantly get sucked back into the loop again!
Any ideas on how to get it to work? Im using one pump on the left hand side looking at the res from the front. I have also got the acrylic piece and serial link, can i use the acrylic piece with one pump as i heard it makes improvements?

Any help is appreciated.

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio
Contact:

Re: Need help with 452 1.3v drivebay res.

Postby Ace0751 » Sun Jul 20, 2014 7:00 pm

What I did to get all the air out is disconnect the hose that is going to the IN inlet and blow into the res. After a bit the flow should start moving, make sure you have a cup with the other hose to drain from. It sounds a bit odd to do something like this but with the 452 it seems like an easy way. It might work for you but its worth a shot, this method gets liquid into the pump and starts the flow thus getting all the air out. It's easier to do with quick disconnects cause once it starts flowing you can turn the PC off and reconnect and turn the PC back on.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case

Izerous
Rain Maker
Rain Maker
Posts: 1183
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada
Contact:

Re: Need help with 452 1.3v drivebay res.

Postby Izerous » Mon Jul 21, 2014 10:45 am

Tilt it backwards so the res is pointing strait up. Open the front plug and fill/prime with it pointing up.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio
Contact:

Re: Need help with 452 1.3v drivebay res.

Postby Ace0751 » Tue Jul 22, 2014 5:00 pm

If the air pocket is in the radiator then they will have a much more difficult time getting it out.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case


Return to “Pumps & Reservoirs”

Who is online

Users browsing this forum: No registered users and 0 guests