These are not the best pictures, things are a bit dusty and messy. And the face plate for the hidden dvd-burner fell off. Haven't had time to re-attach it properly. The UV effects don't' show very well but there are 4 AC Ryan dual over boosts for the UV. And the window is a 2-way mirror so it prevents a crisp image.

I took out the front plastic grill vent thingy. And replaced it with a a mesh. Inside i cut out some of the excess metal between the hard drives and the new fans. Completely removed the 80mm mountings in the hard drive cages, better airflow from the larger fans that way and due to the case's short depth and everything inside gave me a bit more clearance behind the hard drives from being able to move them forward. The 5.25 thing right above the x-fi breakout box is Sunbeam Light bus. Actually works pretty well for controlling everything that I typically have hooked up. The 4 buttons on in the 3.5 drive space. 2 are dvd-roms, and the other 2 controls ram led's. However moving to dominator ram i ditched them.

Bottom rad in this picture is part of the KIT-1000 i purchased. The one that came with the enclosure and the mounting to mount it externally. Top is the 1.2KW Koolance PSU.

Trying to show that the ac ryan's are bright, they actually make the external hosing glow as well. It's Feser black UV and as mentioned before the camera doesn't pickup the UV all that well.

There is a 30 led, led strip right below the window. There was 2x30red and 2x30green however had issues with the glue holding where i placed them so removed them for the time being.