i7 950 is HOT

Post your speeds and temps, or just talk shop.
Uelr
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Dec 06, 2011 3:33 am

i7 950 is HOT

Postby Uelr » Tue Dec 06, 2011 3:40 am

Reservoir and Pump, RP-1005
Radiator, 2x120mm 20-FPI
Fan, 120x38mm, 116CFM
CPU-370 (CPU)
i7 950
The problem im haven is even with the punp and fans wide open and not oced at all im runing 60c across all cores at 25% load

i have reset my block and that did not help at all

any clue on why or help at all

Ace0751
Fire Hydrant Gunner
Fire Hydrant Gunner
Posts: 452
Joined: Sat Apr 09, 2011 8:12 am
Location: Cleveland, Ohio

Re: i7 950 is HOT

Postby Ace0751 » Tue Dec 06, 2011 9:45 am

Does the block have enough pressure on the CPU? Too much or too little will cause it to rise. Also did you put any thermal compound on the CPU? Don't use the koolance stuff have to go with something better.
GIGABYTE X58-UD7 Mobo Rev. 2
Intel i7 950 3.25Ghz
Corsair DOMINATOR GT 12GB 2000mhz DDR3
MSI Radeon 290X
Danger Den Customized Case

Uelr
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Dec 06, 2011 3:33 am

Re: i7 950 is HOT

Postby Uelr » Tue Dec 06, 2011 9:56 am

EVGA Frostbite Thermal Grease for tc and i belive there is enought pressure it is snug to the cpu

JoeM
Water Pistol Grunt
Water Pistol Grunt
Posts: 5
Joined: Mon Aug 15, 2011 7:53 pm

Re: i7 950 is HOT

Postby JoeM » Tue Dec 06, 2011 6:38 pm

There's a lot of stuff that can affect that. Are there big air bubbles in the loop? Maybe trapped in the rad? Res completely full (i.e. pump isn't shooting air bubbles around)? Your fans working correctly on the rad, or is there a fan controller that might not be strong enough to push the high CFM fans in there somewhere? And as Ace mentioned - TIM and pressure can definitely cause it too. Also, you've got high CFM fans with a low FPI rad. You're losing a lot of cooling potential from those fans by not going with a 30-FPI rad. Doubt that's the cause here, but if you're okay with putting up with the noise those suckers make, you might as well get the full benefit from it. Lastly, really dumb question, but I gotta ask - you are reading temps in Celsius, right? Not Fahrenheit? Just making sure, you know... I'd probably do something stupid like that myself. :)

Uelr
Water Pistol Grunt
Water Pistol Grunt
Posts: 3
Joined: Tue Dec 06, 2011 3:33 am

Re: i7 950 is HOT

Postby Uelr » Wed Dec 07, 2011 12:22 am

usen the evga tp. good pressure no kinks no air bubbles usen the Reservoir and Pump, RP-1005. Only thing i can think of is i have the quick disconnects im ordering new conections and inline watr temp to see what the water temp is and go from there

overkill
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Mon Oct 06, 2008 5:25 pm

Re: i7 950 is HOT

Postby overkill » Wed Dec 07, 2011 8:54 am

no clue why it want let me post on uelr but any how
ive checked the block it is tight as for tp i used the EVGA Frostbite Thermal Grease
i dont see any thing that would hint to air traped somewhere as far fan controler in usen the RP-1005


Return to “Hardware and Overclocking”

Who is online

Users browsing this forum: No registered users and 0 guests