TMS-205 fan speed issue

Koolance TMS Software & Hardware Interface...
Gus_Sin
Water Pistol Grunt
Water Pistol Grunt
Posts: 2
Joined: Tue Apr 30, 2013 2:28 am

TMS-205 fan speed issue

Postby Gus_Sin » Tue Apr 30, 2013 3:02 am

Hi,
I recently bought the TMS-205 and it's extension board and connected 6 Corsair SP12 - Quite Edition fans to it. The problem is, I can not seem to slow down the fans all that much. Software show they run at 1350rpm at 100% and they only go down to around 1000rpm at 10%. I had to reduce it to 2 % to get 800-900rpm but I know these fans can run slower than that. So, what's wrong here?
Thanks for the help.

JamesB
Water Pistol Grunt
Water Pistol Grunt
Posts: 6
Joined: Thu Sep 19, 2013 3:19 pm

Re: TMS-205 fan speed issue

Postby JamesB » Thu Sep 19, 2013 3:32 pm

The TMS-205 was only tested to work with Koolance fans. It uses PWM as a signal, and is specific to the spec of Koolance fans.

0% on the TMS-205 is probably low enough to make a Koolance fan stop spinning. It seems your Corsair fans were made to run at a larger range of signal, since they are still at about 800-900rpm at 2%.


Return to “Software”

Who is online

Users browsing this forum: Bing [Bot] and 1 guest