CTR-CD1224 Flow Meter

Fittings, nozzles, quick-disconnects, speed controllers, power supplies, & everything else...
Tornadojoe
Water Pistol Grunt
Water Pistol Grunt
Posts: 1
Joined: Tue May 16, 2017 5:18 pm

CTR-CD1224 Flow Meter

Postby Tornadojoe » Tue May 16, 2017 5:31 pm

I have a Ctr-CD1224.The back shows 4 wire FM-16 2 wire FM-17 connection and in menu, does the FM-18/19 and FM-14 two wire pulse the same ? Or do I have to stick with FM-16/17 ?

Izerous
Rain Maker
Rain Maker
Posts: 1185
Joined: Tue Sep 16, 2008 10:34 am
Location: Edmonton, Canada

Re: CTR-CD1224 Flow Meter

Postby Izerous » Wed May 17, 2017 1:41 pm

If you go to the "Specifications" tab for the following links
FM18
FM17
They both have a frequency vs flow rate chart and you can compare for the other flow meters as well

FM18
Image
FM17
Image

Picking a spot like...
@15Hz
FM18 would be 4.24 LPM
FM17 would be 4.605 LPM

This means if you used a FM18 in the FM17 port it would probably just read a little high. It would display ~4.61 but would really be ~4.24

Now if you look even closer you will see the the FM17 6mm multiplier is 0.28xHz and the FM18 10mm is 0.283. In theory if you hook up a FM18 and set the controller to 6mm tubing (even though you probably have 10mm tubing) it should read just about spot on.
Corsair 800D
2xPMP-450S > Amd FX8370 > Asus CH4-EX > AMD 6990 > AMD 6990 > 2x1080 rads > return
32GB Ram


Return to “Fittings, Nozzles, Quick-Disconnects, Misc.”

Who is online

Users browsing this forum: No registered users and 1 guest